Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

126-150 из 397

Упорядочить:
How are multiple scan lists graphed?
The starting point for each scan list is indicated by a vertical bar on the graph and the label Started.

FAQ 2010-05-05

How can I update the 34980A to Firmware Revision 2.19?

FAQ 2010-05-05

How do I branch from one scan to another?
The Stop the scan and start the scan on action on the “Configure Events” tab, allows you to branch to another scan list on the occurrence of the corresponding event.

FAQ 2010-05-05

How many instruments can I have in a configuration?
You can have up to two 34980As or four 34970As in a configuration

FAQ 2010-05-05

How do I start a scan when using multiple scan lists?
Scanning always starts with the Base scan list.

FAQ 2010-05-05

I don't have channels wired-up yet. How can I experiment with Data Logger Pro?
You can view getting started “simulations” by clicking Help > Start Simulation Mode and selecting a simulation from the list.

FAQ 2010-05-05

Can I mix 34980As and 34970As in the same configuration?
You can have a combination of one 34980A and one or two 34970As in a configuration.

FAQ 2010-05-05

How can I get started using multiple scan lists?
Please refer to the “Getting Started with Multiple Scan Lists, Limits, Events and Action Scripts” in the Help menu.

FAQ 2010-05-05

Can I upload instrument configurations and scanned data from an instrument?
Yes. To upload the instrument configuration and, if available, measured data, click Configuration > New by Upload...

FAQ 2010-05-05

Where can I export the data?
You can save data to files on any disk drive or storage media connected to your PC.

FAQ 2010-05-05

How do I control instruments using SCPI commands?
You can use Action Scripts and SCPI commands to control any instrument connected to the PC.

FAQ 2010-05-05

How do I acquire and install a license?
After the evaluation period, you must license BenchLink Data Logger Pro as described below.

FAQ 2010-05-05

Are there separate licenses for 34970A and 34980A instruments?
Yes. Each instrument uses a specific Data Logger Pro product number.

FAQ 2010-05-05

I'm only interested in some of the scanned data. Can I automatically reduce the data during export?
Yes. You can also reduce data when graphing. See “Data Reduction” in the Help menu for details.

FAQ 2010-05-05

How do multiple scan lists appear in a datalog?
Multiple scan lists are stored by Data Logger Pro in the same datalog.

FAQ 2010-05-05

Can I be scanning and run an Action Script at the same time (in parallel)?
No. Scan lists and Action Scripts are executed sequentially

FAQ 2010-05-05

Can I set a limit on multiple channels?
Yes. After configuring more than one channel limit on the “Configure Scan Lists” tab, you can configure the On Multiple Channel Limits event on the “Configure Events” tab.

FAQ 2010-05-05

Can I reduce data while scanning?
No. All scanned data is saved in the datalog.

FAQ 2010-05-05

How can I Locate Exported Data on the Hard Disk?
You can control where files are stored using either the automatic or manual methods discussed above.

FAQ 2010-05-05

Can scanned data be exported? If so, what formats are supported?
Yes. Data can be exported to files in either ASCII or Unicode format.

FAQ 2010-05-05

Can I have a notification send an email message?
Yes. You can use a notification to execute a custom-written batch file that sends an email.

FAQ 2010-05-05

Is there a pictorial or tabular representation available for my scan lists, events, Action Scripts, and notifications?
Yes.

FAQ 2010-05-05

How can I tell if my PC is licensed?
In Data Logger Pro, click Tools > Licensing > License Status... The “License Status” dialog box displays your PC's license status.

FAQ 2010-05-05

How is licensing implemented for Data Logger Pro?
To run the Data Logger Pro software after the evaluation period, you must have a license for each PC using the software.

FAQ 2010-05-05

How do I set channel limits?
On the “Configure Scan Lists” tab, after configuring a channel's measurement function, you can set limits by clicking in the channel's Limit Type column.

FAQ 2010-05-05

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие