Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

101-125 из 397

Упорядочить:
Why does the voltage range setting on my U2300A switch to auto scale even though I had set the channel to a specific voltage range in the IVI-COM?
The auto scale function is one of the features of the U2300A Data Acquisition (DAQ) devices and is only supported under polling mode….

FAQ 2010-08-09

When I sent commands using VISA (Both Keysight VISA and NI VISA), why must i put '\n' or '\r' after the commands for U2600A…
Please upgrade your U2600A firmware to version 1.05 or above

FAQ 2010-08-09

When using the U2300A/U2500A/U2600A Series Data Acquisition devices, how many modular chassis can the AMM application connect to?
The Measurement Manager (AMM) is designed to operate with one chassis at a time….

FAQ 2010-08-09

What are differences for number of channels that can be displayed under continuous, polling and single shot for U2300A/U2500A?
There is no difference in the number of channels that can be displayed under the continuous, polling and 1 shot modes…

FAQ 2010-08-09

Will I still be able to use the digital I/O function of the U2355A or U2356A if I use this device with the U2802A Thermocouple input device?
No, the digital I/O function of the U2355A or U2356A Data Acquisition (DAQ) device will not be accessible if used with the U2802A device.

FAQ 2010-08-09

I see spikes at the U2351A/U2353A's Analogue Output when Analogue Input is turned on and its frequency changes according to the AI sampling.
There is a spike on the U2351A/U2353A's Analogue Output when Analogue Input is turned on because....

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

For U2300A/U2500A Series Data Acquisition (DAQ) devices, can the Measurement Manager (AMM) display in units other than voltage (v)?
Yes, the Measurement Manager (AMM) can display in units other than voltage (v)….

FAQ 2010-08-08

I get error from the example "C:\Program Files\Keysight\RF Switch Driver\Examples\VS.NET\CSharp\Example1".
The temporary solution to this is to load the U2931A .dll file that was not loaded with the...

FAQ 2010-07-18

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

Why do I get verification error upon reset with single channel pulsed switches and Y1151A distribution board?
On this particular distribution board...

FAQ 2010-06-30

Keysight 34970A FAQ archive
More than 100 FAQs regarding the 34970A data acquisition/switch unit

FAQ 2010-06-07

How can I remotely view what modules are installed in the 34970A?
Use the SYSTem:CTYPe? {100|200|300} SCPI command or System.CardType( ) IVI COM object.

FAQ 2010-05-16

What is the temperature coefficient supported by the 34970A for RTD temperature measurements?
The 34970A supports PT100 RTD's with an alpha=0.00385, RTD's with alpha=0.00385, or alpha=0.00391.

FAQ 2010-05-16

Can the measurements taken be read from the 34980 Data Acquisition Front Panel?
No

FAQ 2010-05-14

No Title
Instead of the ("Counter value"/"48 x 10^6") as the duration in seconds taken to count, it is...

FAQ 2010-05-10

Is number of bits the only factor to look at if I'm measuring at very low voltage say 5mVpp?
No it is not. Often times, you will have to look at the Gain Error and Offset Error as well as...

FAQ 2010-05-10

Transferring Data and Configurations to a new version or to a new computer
Moving between computers with same version or moving configurations and data to a new version on the same computer...

FAQ 2010-05-07

What is an Action Script and what can I do with it?
An Action Script contains one or more action steps that perform actions on modules in 34970A/34980A instruments, and other instrumentation connected to the PC.

FAQ 2010-05-05

How can I move a complete configuration from one PC to another?
You can do this by creating a package, move the package to the new PC then read the package in.

FAQ 2010-05-05

What is the Base scan list?
The default scan list is named Scan List A and is the Base scan list.

FAQ 2010-05-05

Can two scan lists be running at the same time?
No. Only one scan list is active at any given time.

FAQ 2010-05-05

How can I update the 34980A to Firmware Revision 2.19?

FAQ 2010-05-05

Can I have different channels in different scan lists?
You can have different enabled channels in different scan lists.

FAQ 2010-05-05

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие