이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 397

정렬방식:
X8711A – Help file

FAQ 2019-08-27

FILE FILE 421 KB
Does the X8711A support SCPI for remote programming?
The X8711A does not support SCPI. However, an instrument API/driver in .NET DLL is provided. Click on the link for additional information.

FAQ 2019-07-08

How do I install the X8711A software?
Use the installation wizard to install the software, or see the supporting document for manual installation.

FAQ 2018-06-28

Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF. Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states. If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly. To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF. Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.

FAQ 2017-11-13

U2651A / U2652Ar에서 디지털 입력 전압 <24V를 지원할 때 28V 디지털 신호를 U2651A / U2652A에 어떻게 입력 할 수 있습니까?
전압 분배기를 연결...

FAQ 2017-10-25

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

PXI, PXIe 및 AXIe의 데이터 전송 속도는 어떻게됩니까?
PXI-1에는 두가지 경우가 있습니다.

FAQ 2017-05-17

What is the current rating of the Y113xA cables?
The Y1135A and Y1136A cables are 50 conductor, 24 AWG cables with 25 shielded twisted pairs with PVC insulation. They can be used with the 34921A, 23A, 25A, 31A, 32A, 33A, 37A, 38A, 51A, and 52A plug-in modules for the 34980A. However, they do not support the full rated total current of the 34937A and 34938A. The Y1137A and Y1138A cables are 78 conductor cables 28 AWG conductors with 39 shielded twisted pairs. They can be used with the 34922A, 24A, 34A, 39A, and 34950A plug-in modules.

FAQ 2016-12-13

34972A may freeze when LAN connection is under control after power-up
Yes. The first thing to remember is that the 34972A freeze because the user is trying to communicate with the instrument right after power-up. During that time, the instrument is not yet in ready mode. To prevent the problem, please set a delay (approximately 20s or more time until the instrument boot up completely) after power-up before attempting the LAN communication.

FAQ 2016-11-01

34972A with USB data logging may eventually freeze. How to prevent?
Yes, experience has shown that using a powered USB 2.0 Hub between the 34972A and the PC usually eliminates the problem.Using LAN instead of USB is the recommended solution if possible.

FAQ 2016-10-26

Does the L449XA have USB? What interfaces are built in?
LAN and GPIB are included. The 82357B USB/GPIB converter is available if you require USB.

FAQ 2016-07-05

34980A에 알람 설정 시 모니터하고 스캔하는 방법
첨부 VEE 예제 참조하십시오.

FAQ 2016-04-22

IviSwtch API가 지원하는 34980A 스위치 모듈은 무엇입니까?
IviSwtch API가 지원하는 스위치 모듈은 아래와 같습니다.

FAQ 2016-04-22

최대 2000rdgs/sec의 열전대 측정 속도를 얻으려면 어떻게 해야 하나요?
아래 VEE 예제의 SCPI command를 참조하십시오.

FAQ 2016-04-22

34923A 보호 저항(Protection resistors)를 바이패스 하는 방법
34923A 모듈의 100 ohm 저항을 바이패스 하려면 jumper를 연결해야 합니다.

FAQ 2016-04-22

LAN 을 통해 PXI 제품을 사용할수 있나요?
LAN 을 통해 PXI 제품을 사용할수 있나요?

FAQ 2015-04-22

What kind of backplane connectors do the PXI switches have?
PXI 스위치는 어떤 종류의 connector 를 가지고 있나요?

FAQ 2015-04-22

Are all PXIe system modules/controllers compatible with all chassis?
모든 PXI 모듈/컨트롤러는 모든 샤시와 호환이 되나요?

FAQ 2015-04-22

Can I put the Keysight Switch cards into a PXIe chassis?
PXIe 샤시에 Keysight 스위치 카드를 사용할 수 있나요?

FAQ 2015-04-22

U2300A 시리즈 데이터수집장치를 Labview로 동작시키기 위해서 무슨 드라이버가 필요합니까?
IVI-COM 드라이버는 U2300A 시리즈 데이터수집장치를 Labview로 구동하기 위해 필요로 합니다.

FAQ 2015-04-20

U2300A,U2500A 시리즈 DAQ는 리눅스 환경에서 지원되나요?
아니오. U2300A,U2500A 시리즈 DAQ는 리눅스 환경에서 지원되지 않습니다.

FAQ 2015-01-28

34980A 메인 프레임과 모듈, L44xx 시리즈 LXI 스위치와 제어 장치 메모리를 Clear 하려면 어떻게 해야 하나요?
아래 링크된 파일을 참조하십시오.

FAQ 2015-01-28

U2300A, U2500A는 anti-aliasing 필터를 가지고 있는가?
아니오. 키사이트 DAQ는 anti-aliasing 필터를 가지고 있지 않습니다.

FAQ 2015-01-28

Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

1 2 3 4 5 6 7 8 9 10 ... 다음