検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

151-175 / 429

並べ替え
Can I filter the data shown on a graph?
Yes. On a graph tab, click the Channels... button to select which channels to graph and/or to show only certain measurement functions.

FAQ 2010-05-05

Is there a pictorial or tabular representation available for my scan lists, events, Action Scripts, and notifications?
Yes.

FAQ 2010-05-05

How do I control instruments using SCPI commands?
You can use Action Scripts and SCPI commands to control any instrument connected to the PC.

FAQ 2010-05-05

How is licensing implemented for Data Logger Pro?
To run the Data Logger Pro software after the evaluation period, you must have a license for each PC using the software.

FAQ 2010-05-05

I don't have channels wired-up yet. How can I experiment with Data Logger Pro?
You can view getting started “simulations” by clicking Help > Start Simulation Mode and selecting a simulation from the list.

FAQ 2010-05-05

How can I open a configuration from a different data logger application?
See “Import Data Logger 3 Configuration”, or “Import Data Logger for 34980A Configuration”, or “Packages” in the Help menu for detail.

FAQ 2010-05-05

Can I set a limit on multiple channels?
Yes. After configuring more than one channel limit on the “Configure Scan Lists” tab, you can configure the On Multiple Channel Limits event on the “Configure Events” tab.

FAQ 2010-05-05

How can I Locate Exported Data on the Hard Disk?
You can control where files are stored using either the automatic or manual methods discussed above.

FAQ 2010-05-05

How do multiple scan lists appear in a datalog?
Multiple scan lists are stored by Data Logger Pro in the same datalog.

FAQ 2010-05-05

Can I reduce data while scanning?
No. All scanned data is saved in the datalog.

FAQ 2010-05-05

Can two scan lists be running at the same time?
No. Only one scan list is active at any given time.

FAQ 2010-05-05

Where can I export the data?
You can save data to files on any disk drive or storage media connected to your PC.

FAQ 2010-05-05

Are there separate licenses for 34970A and 34980A instruments?
Yes. Each instrument uses a specific Data Logger Pro product number.

FAQ 2010-05-05

Can I send an email following a scan or on some event?
Yes. You can use a notification to execute an external program or batch file in response to an event.

FAQ 2010-05-05

How can I get started using multiple scan lists?
Please refer to the “Getting Started with Multiple Scan Lists, Limits, Events and Action Scripts” in the Help menu.

FAQ 2010-05-05

Can I mix 34980As and 34970As in the same configuration?
You can have a combination of one 34980A and one or two 34970As in a configuration.

FAQ 2010-05-05

Can I have different channels in different scan lists?
You can have different enabled channels in different scan lists.

FAQ 2010-05-05

Can I have a notification send an email message?
Yes. You can use a notification to execute a custom-written batch file that sends an email.

FAQ 2010-05-05

Can I use the National Instruments 34970A LabView Driver and Examples with the 34972A?
Yes, there is a new Labview driver that supports both the 34972A and the 34970A...

FAQ 2010-04-16

Why USB modular instruments (U272XA, U2741A, U2751A and U2761A) is not detectable by E5813A?
PC is failed to enumerate the USB modular instrument.

FAQ 2010-04-09

Transferring Data and Configurations to a new version or to a new computer
Moving between computers with same version or moving configurations and data to a new version on the same computer:

FAQ 2010-03-30

Is U2751A compatible with E5813A?
U2751A is not compatible with E5813A.

FAQ 2010-03-22

Is the USB connection of U2300A,U2500A and U2600A optically coupled?
No. It is not.

FAQ 2010-03-22

34970A: Is there a battery in the Keysight 34970A?
Yes. the 34970A contains an internal battery that provides power to the internal real-time clock, stored states, and reading storage memory when the instrument ac line power is removed.

FAQ 2010-01-12

What does ENOB of 13.3 bit means in the specification sheet?
ENOB = (SINAD-1.76)/6.02 Overall Accuracy = ENOB (Effective Number of Bits)....

FAQ 2009-12-15

前へ 1 2 3 4 5 6 7 8 9 10 ... 次へ