Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 395

Sort:
DAQ970A/DAQ973A: Why do I constantly get an Error -310 when I turn on the instrument? How can I clear the error?
The error -310 only happens when your instrument with firmware version 2.01 has been previously turned off for more than 10 minutes.

FAQ 2020-02-19

X8711A – Help file

FAQ 2019-08-27

FILE FILE 421 KB
Does the X8711A support SCPI for remote programming?
The X8711A does not support SCPI. However, an instrument API/driver in .NET DLL is provided. Click on the link for additional information.

FAQ 2019-07-08

How do I install the X8711A software?
Use the installation wizard to install the software, or see the supporting document for manual installation.

FAQ 2018-06-28

Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF. Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states. If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly. To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF. Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.

FAQ 2017-11-13

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

What is the current rating of the Y113xA cables?
The Y1135A and Y1136A cables are 50 conductor, 24 AWG cables with 25 shielded twisted pairs with PVC insulation. They can be used with the 34921A, 23A, 25A, 31A, 32A, 33A, 37A, 38A, 51A, and 52A plug-in modules for the 34980A. However, they do not support the full rated total current of the 34937A and 34938A. The Y1137A and Y1138A cables are 78 conductor cables 28 AWG conductors with 39 shielded twisted pairs. They can be used with the 34922A, 24A, 34A, 39A, and 34950A plug-in modules.

FAQ 2016-12-13

34972A may freeze when LAN connection is under control after power-up
Yes. The first thing to remember is that the 34972A freeze because the user is trying to communicate with the instrument right after power-up. During that time, the instrument is not yet in ready mode. To prevent the problem, please set a delay (approximately 20s or more time until the instrument boot up completely) after power-up before attempting the LAN communication.

FAQ 2016-11-01

34972A with USB data logging may eventually freeze. How to prevent?
Yes, experience has shown that using a powered USB 2.0 Hub between the 34972A and the PC usually eliminates the problem.Using LAN instead of USB is the recommended solution if possible.

FAQ 2016-10-26

Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Keysight and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How can I make NI LabVIEW communicate with Keysight 82357B USB/GPIB Interface?
Keysight IO Libraries install as secondary VISA side by side with NI VISA. Keysight IO Libraries Keysight 488 Options enable. In NI MAX, ensure Passport for Tulip (NIVisaTulip.dll) enable.

FAQ 2014-04-17

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Can the L4490A/L4491A mainframe be password protected when using LAN?
Yes, instructions for using password protection can be found in the web interface.

FAQ 2014-04-07

What type of internal memory is installed into the 34972A LXI Data Acquisition Switch Unit?
The Keysight 34972A LXI Data Acquisition Switch Unit utilizes Windows CE...

FAQ 2014-04-07

How do you clear the 34980A multifunction switch/measure mainframe and modules, L44xxA series LXI switch and control instruments memories?
Please refer to the documents for a comprehensive listing of memory installed into these products.

FAQ 2014-04-07

My Keysight LXI based SICL / LAN instrument is timing out on the LAN connection under automation control. Is it possible to avoid this LAN timeout?
Yes, please access the LXI based instruments web server by entering the instruments IP address into a web browser. If the LAN has timed out it maybe necessary to cycle the power button.

FAQ 2014-01-28

Which 34980A Switch Modules are supported by the IviSwtch api?
All modules except the 34945A, 34950A, 34951A, 34952A, 34959A...

FAQ 2014-01-22

What components are included in the Keysight Y1159A cable kit?
The Keysight Y1159A is a 16 pin IDC to 16 pin IDC cable kit for the Y1150A, Y1151A, Y1152A, Y1153A, Y1154A and / or the Y1155A distribution boards. (See Chart)

FAQ 2013-12-11

What components are included in the Keysight Y1158A cable kit?
The Keysight Y1158A is a 10 pin IDC to 10 pin IDC or 10 pin IDC to 14 pin IDC cable kit for the Y1153A and / or the Y1154A distribution boards. (See Chart)

FAQ 2013-12-11

What components are included in the Keysight Y1157A cable kit?
The Keysight Y1157A is a 9 pin DSUB to 10 pin IDC cable kit for the Y1150A, Y1152A and / or the Y1154A distribution boards. (See Chart)

FAQ 2013-12-11

Can I do voltage measurement using the U2802A rather than temperature measurement?
Yes, you can do voltage measurement easily by using the Keysight Measurement Manager (AMM)...

FAQ 2013-11-17

What’s the difference between E5810B and E5810A?
Please refer to the table for side-by-side comparison below

FAQ 2013-10-25

Why don’t my Keysight PXI modules show up in National Instruments-Measurement & Automation Explorer (NI-MAX)?
Older versions of Keysight and other vendor’s PXI software could result in Keysight modules not appearing in NI Max....

FAQ 2013-08-30

1 2 3 4 5 6 7 8 9 10 ... Next