Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

1-25 из 147

Упорядочить:
Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How can previously created data in BenchLink II be exported?
Open a previously saved configuration file with data and then export the data as a Text (.txt) file or Comma Separated values (.csv) file.

FAQ 2012-11-05

How many Keysight 34970A data acquisition units can be connected to a single PC at a time?
Only one Keysight 34970A can be connected for each RS-232 port on the PC. A GP-IB cable can be used to connect up to 15 units if the GP-IB cable is being referenced by the VEE software. The Benchlink Data Logger 3 software can support up to 4 units...

FAQ 2012-01-25

Can Excel control a scan, and make and record measurements using the 34970A?
Use the 34970A IntuiLink add-in, Excel Macro language, or the Instrument Code Wizard.

FAQ 2011-12-20

Why does BenchLink DataLogger 3 generate the "MDAC installation failed" error message?
The MDAC (Microsoft Data Access Components) may be corrupted and needs to be repaired.

FAQ 2011-12-20

The Benchlink Data Logger Software is unable to see my 34970A even though it is connected, how do I correct this?

FAQ 2011-12-20

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

34970A: How do I add a DMM to a 34970A that does not have one installed?
Order the customer installable retrofit kit 34970-80100.

FAQ 2010-10-12

How do I rack mount two instruments of different depths?
There are three ways to rack instruments of different depths side-by-side; for example, a Keysight 33220A with a Keysight 34401A.

FAQ 2010-10-12

Transferring the license from an older version to version 3.00
Before updating to a new revision of Data Logger on the SAME computer, be certain to save all data and configuration files that you wish to keep.

FAQ 2010-09-19

Can I retrieve data from the 34970A while it is scanning?
No. You can collect data during a scan, stop the scan and then transfer the data.

FAQ 2010-09-09

How can I copy Channels to Other Channels in BenchLink 3?
Select the channel(s) to be copied, right-click and select copy, select the channel(s) to be pasted, right click and select paste.

FAQ 2010-09-08

Why does BenchLink 3 generate the "Object reference not set to an instance of an object" error?
This error is caused by corruption in the .NET Framework

FAQ 2010-09-08

Keysight 34970A FAQ archive
More than 100 FAQs regarding the 34970A data acquisition/switch unit

FAQ 2010-06-07

How can I remotely view what modules are installed in the 34970A?
Use the SYSTem:CTYPe? {100|200|300} SCPI command or System.CardType( ) IVI COM object.

FAQ 2010-05-16

What is the temperature coefficient supported by the 34970A for RTD temperature measurements?
The 34970A supports PT100 RTD's with an alpha=0.00385, RTD's with alpha=0.00385, or alpha=0.00391.

FAQ 2010-05-16

Transferring Data and Configurations to a new version or to a new computer
Moving between computers with same version or moving configurations and data to a new version on the same computer...

FAQ 2010-05-07

What is an Action Script and what can I do with it?
An Action Script contains one or more action steps that perform actions on modules in 34970A/34980A instruments, and other instrumentation connected to the PC.

FAQ 2010-05-05

How can I move a complete configuration from one PC to another?
You can do this by creating a package, move the package to the new PC then read the package in.

FAQ 2010-05-05

What is the Base scan list?
The default scan list is named Scan List A and is the Base scan list.

FAQ 2010-05-05

Can two scan lists be running at the same time?
No. Only one scan list is active at any given time.

FAQ 2010-05-05

Can I have different channels in different scan lists?
You can have different enabled channels in different scan lists.

FAQ 2010-05-05

What are channel limits?
Limits can be set on multiplexer, totalizer and digital read channels (see the limit types question below).

FAQ 2010-05-05

How are multiple scan lists graphed?
The starting point for each scan list is indicated by a vertical bar on the graph and the label Started.

FAQ 2010-05-05

How do I branch from one scan to another?
The Stop the scan and start the scan on action on the “Configure Events” tab, allows you to branch to another scan list on the occurrence of the corresponding event.

FAQ 2010-05-05

1 2 3 4 5 6 Следующие