Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 31

Упорядочить:
Where do I download the mechanical drawings for the M9506A?
Files can be imported into your modeling application.

FAQ 2019-09-10

How to upgrade your Embedded Controller to Windows 10
You can easily update your Embedded Controller to Windows 10 by swapping out the SSD with a new Windows 10 SSD.

FAQ 2018-06-07

What is the Embedded Controller Default Password? Answer: Keysight4u!
The default password is “Keysight4u!” for the Administrator account for Windows 10 Enterprise 2016 LTSB. We recommend that you change the password for improved security, because the default password is public knowledge.

FAQ 2017-11-14

Where do I download the mechanical drawings for the M9537A?
Files can be imported into your modeling application.

FAQ 2016-11-16

How do I setup for DisplayPort Hot Swap capability?
The M9537A has 3 DisplayPorts that are activated on boot-up. If you move a cable from one DisplayPort to another, you must reboot to activate the new configuration.

FAQ 2016-11-16

Where do I download the mechanical drawings for the M9502A?
Files can be imported into your modeling application.

FAQ 2016-11-16

How do I make the AXIe module show up when there is an empty slot between it and the controller?
If you leave an empty slot between the M9537A controller and an AXIe module, you might not be able to use the AXIe module and an error will show up in Windows Device Manager.

FAQ 2016-11-16

How do I fix: unable to change GPIB settings on an M9037A or M9537A Embedded Controller?
Make the following changes...

FAQ 2016-08-27

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

Where do I download the mechanical drawings for the M9514A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9505A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9521A?
Files can be imported into your modeling application.

FAQ 2016-01-08

How do I connect multiple PXIe and/or AXIe chassis together with a single controller?
PXIe and AXIe chassis can be interconnected in multiple configurations.

FAQ 2013-08-07

Why does the chassis Soft Front Panel (SFP) not start when I connect to the chassis with my Windows XP PC?
The Keysight PXIe and AXIe chassis require Microsoft .NET Framework 3.5 SP1 installed on the PC in order for the SFP to work. Windows XP does not have this loaded automatically. If you are using a Windows XP PC, please install Microsoft .NET Framework 3.5 SP1 from Microsoft website.

FAQ 2013-07-10

Why is my M9502A or M9505A Soft Front Panel (SFP) displaying error “Unable to open instrument. Driver initialization failed.”
A 32-bit mDNS responder is required for 32-bit applications running on a 64-bit OS when using IOLS 16.2. Installing the 32-bit mDNS responder patch below will add a 32-bit mDNS responder to appropriately resolve mDNS names to an IP address for these applications.

FAQ 2012-10-10

What changed in the Fan Control for the M9502A and M9505A with firmware 1.3.23?
The Fan Speed parameter changed from 8-15 to 35-100.

FAQ 2012-03-27

Keysight Driver Migration Tool

FAQ 2012-01-20

How do you clear the M9502A and M9505A AXIe Chassis memory?

FAQ 2011-07-08

Which computers has Keysight tested with PXI or AXIe chassis?
Keysight maintains a list of tested computers...

FAQ 2011-03-14

Do these products appear in the Keysight connection expert?

FAQ 2010-10-11

What is the data transfer rate of PXI, PXIe, and AXIe?
PXI-1 has two variants...

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

Will ExpressVIs work with Keysight hardware?
No. Keysight has VIs available to use with LabView but not ExpressVIs.

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06

1 2 Следующие