Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 83

Упорядочить:
Firmware update error with "Cannot Open another Window"
I cannot update the firmware with the error message; "Cannot Open another Window"

FAQ 2016-08-04

Can I use N1294A-021/022 low noise filters with B2901A/02A/11A/12A SMU?
No, they aren't recommended to be used with the Keysight B2901/02/11/12A SMUs.

FAQ 2013-09-16

How can the B2900A Series of SMU source pulses whenever it receives an external trigger signal?
It can do it by configuring a digital I/O pin to be used for an external trigger signal. Click the above link for details.

FAQ 2013-09-16

How to use the interlock to output more than ±42V?
B2900A has interlock detection with the digital I/O on the rear pannel. Click the link for details.

FAQ 2013-09-16

Does the B2900A Series of SMUs have Source Memory Sweep Function?
No, the B2900A Series of SMUs doesn't have Source Memory Sweep Function as Keithley 2400 has.

FAQ 2013-09-16

What is the difference among Trigger Types on Single View?
Click the above link for details.

FAQ 2013-09-16

Can the B2900A Series of SMU sweep voltage source by the know on the front panel?
Yes, it's possible by enabiling Immediate V/I Update function. Click the above link for details.

FAQ 2013-09-16

What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?
It should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous. Once you send it with the parameter "ON", the parameter is set to "END VALUE".

FAQ 2013-09-16

What is the difference among data query commands such as ":FETCh?", ":MEASure?", ":READ?", :SENSe:DATA?"?
They have the function to query data similarly but there is some difference among them. Click the above link for details.

FAQ 2013-09-16

How can I set up Power-on State of the B2901/02/11/12A?
It is possible to store the desired instrument condition as Power-on State. Click the above link for details.

FAQ 2012-11-21

Can I use the triaxial cable with B2900A?
Yes. You can use the triaxial cable by using the N1294A adaptor.

FAQ 2012-11-20

Does the B2901/02/11/12A have any search function?
No, the B2901/02/11/12A doesn't have any search function which the analyzers such as the B1500A have.

FAQ 2012-10-09

The channel 2 in the B2902A or B2912A doesn't receive any SCPI commands.
The instrument may be configured to use the conventional command set. Click the above link for details.

FAQ 2012-10-09

I cannot store the channel 2 measurement condition to USB memory stick, why not?
The instrument may be configured to use the conventional command set. Click the above link for details.

FAQ 2012-10-09

The password is required to access the instrument.
The password is required to access the instrument compliant with the LXI specification. Click the above link for details.

FAQ 2012-10-09

How to determine the frequency for Sin function of Quick IV List Sweep?
Frequency = 1 / ( (360 [degree] / X Step [degree]) * Trigger Period )

FAQ 2012-10-09

How can I configure to output continuous arbitrary waveform?
Click the above link for details.

FAQ 2012-03-26

How to configure the time constant of the output filter with the B2901/02/11/12A?
The time constant of the output filter can be configured on the Output Filter dialog box. Click the above link for details.

FAQ 2012-02-01

How can I select the default command set as the remote control command set of the B2901/02/11/12A?
You can configure the unit to use the default command set by pressing the System>SCPI functuion keys. Click the above link for details.

FAQ 2012-02-01

How can I find the remote control command setting of the B2901/02/11/12A?
You can find the remote control command setting by pressing the System>SCPI functuion keys. Click the above link for details.

FAQ 2012-02-01

How can I find the power-on state setting of the B2901/02/11/12A?
You can find the power-on state setting on the System Start-up dialog box. Click the above link for details.

FAQ 2012-02-01

How can I find the power-on program setting of the B2901/02/11/12A?
You can find the power-on program setting on the System Start-up dialog box. Click the above link for details.

FAQ 2012-02-01

How can I configure Trigger Output Signals with the B2901/02/11/12A?
Click the above link for details.

FAQ 2012-02-01

Is there any way to reset only the specified channel of the B2902/12A?
No, there is no way to reset only the specified channel.

FAQ 2011-12-01

How can I realize an accurate low current measurement with the B2901/02/11/12A?
It is necessary to take care of the folloing points in order to make it. Click the above link for details.

FAQ 2011-12-01

1 2 3 4 Следующие