検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 49

並べ替え
89600Sベクトル・シグナル・アナライザ用のE273xAチューナとE273xBチューナの違いは何ですか?
詳細は下記の本文をご覧ください。

FAQ 2005-03-07

マルチフレームCサイズVXIシステムを構築するには?
マルチフレームVXIシステムを構築するには、複数のVXIメインフレーム(E1401B、E8401A、E8403A、E8404A、E8408A)を選択します。

FAQ 2004-07-28

E8408A用のラックマウントのパーツ番号を教えてください。
E8408A VXIカード・ケージをラックマウントする場合、E8397Aラックマウント/ケーブル・ルート・アダプタ・キットとともに1494-0413ラック・スライド・キットまたはE3663ACレールが必要です...

FAQ 2004-06-28

E8401A/E8403A マニュアルは入手できますか?
E8401A, E8403A User and Service Manual は弊社のウェブサイトからPDFファイルとして入手できます...

FAQ 2004-06-28

E1406A: Is there a way to control the E1406A from a LAN connection?
Use the E5810A LAN to GPIB converter.

FAQ 2004-06-15

E1330B: What is the difference between Model E1330B and Model E1458A?
Model E1330B has 4 ports; and the Model E1458A has 12 ports. The E1458A can input while outputting on a port.

FAQ 2004-06-15

E1458A: Where can I find more information on the Model E1458A connector pin out assignments?
See Chapter 2 in the Model E1458A Users Manual

FAQ 2004-06-09

E1330B: What is the difference between Models E1330B, E1458A and E1451A/E1452A?
Models E1451A/E1452A have 64K card memory. Models E1330B and E1458A have only one memory location.

FAQ 2004-06-03

What is the difference between the E1330B and E1458A?
The E1330B has 4 ports, the E1458A has 12 ports. The E1458A can input while outputting on a port.

FAQ 2004-05-28

3488A、3499A/B/C用マイクロウェーブ・スイッチ・ドライバ、44476Bにマウント可能なスイッチのモデルは何でしょうか?
8762A/オプション011等が使用可能です。

FAQ 2003-01-16

E6432A: Application Programs for the Plug&Play Driver

FAQ 2002-10-10

HP E6432A: The National Instruments AT-MXI interface and MXI-1 slot 0 controller

FAQ 2002-10-10

E6432A: Equipment Needed To Generate Signals

FAQ 2002-10-10

HP E6432A: Using an HP E1406A VXI Controller to Operate the Synthesizer

FAQ 2002-10-10

Is PCMCIA for FireWire, E8491B, available?
Yes, please visit the IO Libraries support of IEEE 1394 CardBus Cards.

FAQ 2002-10-07

Where do embedded PCs fit with FireWire E8491B?
Embedded PCs are still faster in small block transfers and some users like embedded PCs because of their small form factor.

FAQ 2002-09-17

If I have a PC with built-in FireWire interface, how can I be sure it will work with the Keysight E8491B?
For best performance we recommend using the host adapter (PCI) card shipping with the E8491B.

FAQ 2002-09-17

Do customers need the enhanced monitor on the E8404A?
The enhanced monitor provides: A better environment for calibrated measurements by utilizing closed loop cooling control.

FAQ 2002-09-17

Can 3488A programs run on 3499A/B/C?
The 3499A/B/C is both hardware and software compatible with the 3488A Switch/Control unit.

FAQ 2002-09-05

How Many Channels of 12A Can the E8480A Switch When Using the E8404A?

FAQ 2002-06-27

Does E8482A supply VEE/LabVIEW drivers?

FAQ 2002-06-27

What kind of framework does E8481A support?

FAQ 2002-06-27

Does E8483A support E8491B(IEEE-1394 PC link to VXI)?

FAQ 2002-06-27

What kind of drivers are supplied with the E8481A?

FAQ 2002-06-27

What is E1472A mode of E8482A?

FAQ 2002-06-27

1 2 次へ