Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-10 из 10

Упорядочить:
Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Why does the error message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear…
The message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear because….

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

Is U2300A and U2500A series DAQ supported in Linux environment?
No. U2300A and U2500A are not supportable in Linux environment.

FAQ 2009-08-06

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

What is the required operating system for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices?
The operating system required for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices is….

FAQ 2008-09-25

Does the Measurement Manager (AMM) run on a Linux operating system?
No, the Measurement Manager (AMM) does not run on a Linux operating system.

FAQ 2008-09-25