検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-10 / 10

並べ替え
Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

[仕様] USBモジュラ型測定器は、Windows7をサポートしていますか?
はい、最新のKeysight Measurement ManagerにてWindows7 32bitをサポートしています。

FAQ 2013-06-24

[仕様] Keysight Measurement Managerは、Windows Vistaでサポートされていますか?
はい、Keysight Measurement Manager バージョン 1.8.3.0以上にて、Windows Vista(Service Pack 1、Business, Ultimate, Enterprise, Basic, Home Premium Editionの各種パッケージ)をサポートしています。

FAQ 2010-11-03

[仕様] Keysight Measurement Manager (AMM) は、英語以外の言語設定もサポートしますか。
はい、Keysight Measurement Manager (AMM) は、英語以外の言語設定もサポートします。

FAQ 2010-11-02

Why does the error message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear…
The message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear because….

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

Is U2300A and U2500A series DAQ supported in Linux environment?
No. U2300A and U2500A are not supportable in Linux environment.

FAQ 2009-08-06

What is the required operating system for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices?
The operating system required for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices is….

FAQ 2008-09-25

USB DAQソフトウェアはLinuxオペレーティング・システムで動作しますか?
動作しません。

FAQ 2008-09-23