Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-16 of 16

Sort:
Can I do voltage measurement using the U2802A rather than temperature measurement?
Yes, you can do voltage measurement easily by using the Keysight Measurement Manager (AMM)...

FAQ 2013-11-17

How can I input 28V digital signal to U2651A/U2652A when it support digital input voltage < 24V?
You can connect a voltage divider in front of the digital input to reduce the voltage to <24V

FAQ 2010-10-07

How do I extract the 32Mpts from U270xA?
One way of “viewing” the full memory waveform is using the zoom function (that the red arrow...

FAQ 2010-09-14

If I set Channel 1 of U2300A/U2500A with voltage range of 5V, I get a reading of 4.99968 when nothing is connected to the DAQ.
If you don't have anything connected to the DAQ and you do an acquisition out of it, the result…

FAQ 2010-08-09

Why do we see unused port in U2300A/U2500A with similar waveform and frequency but with lower amplitude to its adjacent or close by used port?
It is recommended to ground all the AI connection that is not being used. If you have multiples of AI channels to be used, one good way is to have…

FAQ 2010-08-09

What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

No Title
Instead of the ("Counter value"/"48 x 10^6") as the duration in seconds taken to count, it is...

FAQ 2010-05-10

Is number of bits the only factor to look at if I'm measuring at very low voltage say 5mVpp?
No it is not. Often times, you will have to look at the Gain Error and Offset Error as well as...

FAQ 2010-05-10

Is there any special setting that I need to do in Keysight VEE before using the U2300A or U2500A DAQ with it?
Yes. In fact it is the most important thing you need to set before using the DAQ with Keysight VEE. As most instruments uses MSB byte ordering, DAQ...

FAQ 2009-12-15

What is the main difference between the digital output (DO) of the U2100A, U2600A, U2300A and U2500A?
The DO port of U2100A and U2600A requires external power supply to be pumped into the port...

FAQ 2009-10-20

How much of data points from my data acquired can I save into one file?
What we observed is that if you log your file into *.csv file, the most no. of points you will be capturing is 65536 points. However, if you are saving into *.txt file, it will depend on the type of...

FAQ 2009-09-29

How do I know what is the best sampling rate to use for my measurement?
Typically if you follow Nyquist theory, your sampling rate should be 2x the highest frequency of the incoming signal that you are measuring. However, we recommend that you use 5x...

FAQ 2009-09-29

Can U2651A work with 3.3V input signal or not?
As long as there is a potential exceeding 10V and less than 24V between DIin and DIcom, the digital input should be able to observe the incoming signal as logic high...

FAQ 2009-09-29

Why do I receive an error message below ?
Generally, if you are sampling at 60kSa/s and above, you should use high sampling mode to acquire data. This is just a rough guideline. If you encountered this message even when....

FAQ 2009-08-06

How can I remotely connect to all my USB DAQ devices, Digital IOs, and card cage?
Please make sure that your remote PC (which is connected to all your USB instruments) is connected to the same network as yourself. However, your remote PC cannot be connected...

FAQ 2009-08-06

Why should I use the U2802A Thermocouple input device?
The U2802A Thermocouple input device offers you a complete temperature measurement solution when used with data acquisition (DAQ) devices….

FAQ 2008-09-24