Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

76-98 of 98

Sort:
Is the Universal Serial Bus (USB) interface a good choice for data acquisition applications?
The Universal Serial Bus (USB) interface is ideal for data acquisition applications because USB offers plug-and-play capabilities….

FAQ 2008-09-25

What is the lowest sampling rate that can be set for the U2300A/U2500A Series USB Data Acquisition (DAQ) devices?
The Keysight U2300A/U2500A Series Data Acquisition (DAQ0 devices can support sampling rates as low as 3Sa/s.

FAQ 2008-09-25

When using the U2300A Series Multifunction Data Acquisiton (DAQ) devices, how do I implement a command to output a defined voltage value?
When using a U2300A Series Multifunction Data Acquisiton (DAQ), you can configure an output channel to produce a defined voltage value by….

FAQ 2008-09-25

Do the U2300A USB data acquisition (DAQ) devices have DMA channels?
No. The U2300A Series DAQ devices are USB interface devices therefore, they do not have any DMA channels.

FAQ 2008-09-25

Does the Measurement Manager (AMM) run on a Linux operating system?
No, the Measurement Manager (AMM) does not run on a Linux operating system.

FAQ 2008-09-25

What is the maximum distance allowed between a host computer and USB Data Acquisition (DAQ) devices?
According to USB specifications, the maximum distance allowed between a host computer and USB Data Acquisition (DAQ) device is five meters.

FAQ 2008-09-25

Is calibration required for the U2651A/U2652A/U2653A Digital I/O device?
No, calibration is not required for the U2651A, U2652A and U2653A Digital I/O devices.

FAQ 2008-09-24

Can the U2300A/U2500A Series Data Acquisition (DAQ) devices that are used with three modular chassis be synchronized?
Yes, the U2300A and U2500A Series Data Acquisition (DAQ) devices that are used with three modular chassis can be synchronized….

FAQ 2008-09-24

Are there any sample programs provided for the U2300A and U2500A Series Data Acquisition (DAQ) devices?
Yes, sample programs of VEE, LabView and Microsoft® Visual Studio® are available for the U2300A and U2500A Series Data Acquisition (DAQ)….

FAQ 2008-09-24

What are the maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices?
The maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices are:….

FAQ 2008-09-24

How many U2781A modular chassis can be connected via USB at the same time?
USB has a limit of 127 device connections. Theoretically, about 18 chassis can be connected at a time.

FAQ 2008-09-24

Can the Measurement Manager (AMM) application software be used to control all six USB Data Acquisition (DAQ) devices in a modular chassis?
Yes, the Measurement Manager (AMM) can be configured to control all USB Data Acquisition (DAQ) devices in the chassis.

FAQ 2008-09-24

What are the drivers needed to run the U2300A Series Data Acquisition (DAQ) devices with LabView?
The IVI-COM driver is required for the U2300A Series Data Acquisition (DAQ) devices to work with LabView.

FAQ 2008-09-24

When using the U2300A Series DAQ devices, how many channels can the Measurement Manager (AMM) display?
The Measurement Manager (AMM) can display all 16 or 64 channels depending on the model of the U2300A Series DAQ device selected….

FAQ 2008-09-24

Can the U2531A/U2541A/U2542A Data Acquisiton device work in both Single-Ended and Differential mode?
No, the U2531A, U2541A and U2542A Data Acquisiton devices cannot work in both Single-Ended and Differential mode….

FAQ 2008-09-24

What programming platforms are compatible with the U2300A Series Data Acquisition (DAQ) devices?
Keysight VEE, LabView, Microsoft Visual Studio and C++ are compatible with the U2300A Series Data Acquisition (DAQ) devices.

FAQ 2008-09-24

What is the expected transfer rate over the U2781A USB Modular Instrument Chassis?
The transfer rate of the U2781 is dependent on the type of USB Data Acquisition (DAQ) Modules installed and the number of channel counts….

FAQ 2008-09-24

Can the Measurement Manager (AMM) display multiple U2781A modular chassis on the same application window?
No, the Measurement Manager (AMM) can only display one U2781A modular chassis on one application window…

FAQ 2008-09-24

Where can I get the terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices?
The terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices can be found in the User’s Guide….

FAQ 2008-09-24

Which thermocouple types are compatible with the U2802A Thermocouple input device?
Eight standard thermocouple types defined in the NIST ITS-90 Thermocouple Database are compatible with the U2802A input device….

FAQ 2008-09-24

How do I connect external sensors to the U2300A Series Data Acquisition (DAQ) devices?
External sensors can be connected to the U2300A Series Data Acquisition (DAQ) devices through the U2901A or U2902A terminal block….

FAQ 2008-09-24

Why should I use the U2802A Thermocouple input device?
The U2802A Thermocouple input device offers you a complete temperature measurement solution when used with data acquisition (DAQ) devices….

FAQ 2008-09-24

Can the Measurement Manager (AMM) display more than 10 channels for synchronization?
No, the Measurement Manager (AMM) cannot display more than 10 channels for synchronization….

FAQ 2008-09-22

Previous 1 2 3 4