Technical Support
Electronic Measurement
Refine the List
By Type of Content
-
Drivers, Firmware & Software
- Programming Example
By Product Category
-
All Product Categories
-
Modular Instruments
- PXI Products
-
Modular Instruments
1-25 of 26
Get *IDN? Query Results, VISA COM library, C#
This sample program sends a *IDN? SCPI query to an instrument to get its identification string. The result is displayed on a MS Windows Console.
Programming Example 2017-04-28 |
![]() |
Get Lister Data, VISA library, Python 3.5
This script is a reference and starting point for automating Lister data capture over USB.
Programming Example 2017-04-28 |
![]() |
Get *IDN? Query, Screen Image, and Waveform Data Results, VISA COM library, VBA
This sample program performs three different tasks: 1) sends a *IDN? query to the instrument and reads back the ID string, 2) captures and saves a screen image from the oscilloscope, and 3) gets the oscilloscope's waveform data from channels 1 and 2.
Programming Example 2017-04-28 |
![]() |
Get Screen Image, VISA library, Python 3.5
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.
Programming Example 2017-04-28 |
![]() |
Get Segmented Memory Time Tags and Measurement Results, VISA COM library, VBA
This sample program assumes the oscilloscope has been set to capture N segments. The program lists the segment number and the relative time stamp of that segment. A Delay measurement is made between channels 1 and 2 within each segment and the measurement value from each segment is listed.
Programming Example 2017-04-28 |
![]() |
Get InfiniiVision X-Series Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion X-Series oscilloscope.
Programming Example 2017-04-28 |
![]() |
Get Screen Image, VISA library, Python (2.7)
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.
Programming Example 2017-04-28 |
![]() |
Get Segmented Memory Time Tags and Measurement Results, VISA library, Python
This script figures out how many segments were acquired, flips through them, gathers the time tags and desired measurement results.
Programming Example 2017-04-28 |
![]() |
Acquisition Synchronization, Two Simple Methods, VISA library, Python
This script shows the two best synchronization methods for all InfiniiVision and InfiniiVision X-Series oscilloscopes. Benefits and drawbacks of each method are described.
Programming Example 2017-04-28 |
![]() |
Get InfiniiVision Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion oscilloscope.
Programming Example 2017-04-28 |
![]() |
Get Segmented Memory Time Tags, Waveforms, and Measurement Results, VISA library, Python
This script can get waveforms and measurements from analog channels for segmented memory already acquired on an InfiniiVision oscillocope. It can also get time tags and produce an averaged segment for each analog channel.
Programming Example 2017-04-28 |
![]() |
Acquisition Synchronization, Two Simple Methods, MATLAB
This script shows how to properly initialize a Keysight InfiniiVision or InfiniiVision X-Series oscilloscope and synchronize an acquisition using the blocking :DIGitize command.
Programming Example 2017-04-28 |
![]() |
Save and Recall Setups, VISA library, Python
This script shows how to query the oscilloscope setup, save it to disk, recall it form disk, and use it to set up the oscilloscope again. This is also shown using the *LRN? query and with just trigger setups.
Programming Example 2017-04-28 |
![]() |
Get Screen Image and Waveform Data and Save to USB Thumb Drive, VISA library, Python
This script shows how to save a screen image and waveform data to a USB stick, with error checking.
Programming Example 2017-04-28 |
![]() |
Save Multiple Waveforms to a Binary File with Averaging, VEE
This sample program saves multiple waveforms to a binary file with averaging.
Programming Example 2017-04-28 |
![]() |
Load Arbitrary Waveform Data into WaveGen, VISA library, Python
This example shows several methods for getting arbitrary waveform data into the waveform generator of a Keysight InfiniiVision X-Series oscilloscope. The oscilloscope must have the WaveGen license and support arbitrary waveforms.
Programming Example 2017-04-28 |
![]() |
Get Waveform Data, VISA COM library, VBA
This sample program gets waveform data from the oscilloscope.
Programming Example 2017-04-28 |
![]() |
Get Waveform Data, VEE
This sample program gets waveform data from the oscilloscope.
Programming Example 2017-04-28 |
![]() |
Get Waveform Data, LabVIEW
This sample program gets waveform data from the oscilloscope.
Programming Example 2017-04-28 |
![]() |
Get Waveform Data (Elegant), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.
Programming Example 2017-04-28 |
![]() |
Get Waveform Data (Brute Force), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.
Programming Example 2017-04-28 |
![]() |
I/O Libraries Example Programs
Examples to get you started with instrument programming...
Programming Example 2016-10-19 |
|
M9392A Multichannel Streaming Example Program
Sample program, created using Microsoft Visual Studio C#, allows you to begin making multichannel streaming measurements immediately. The source code shows which IVI COM command sequences are required and which test techniques are recommended. The solution can be built on a 32-bit operating system (OS); however, a 64-bit OS is recommended. For details about the program, read the included MCStreamingHelp.pdf file.
Programming Example 2012-04-26 |
![]() |
M9392A Example Programs
Example programs for the M9392A PXI Vector Signal Analyzer. These programs are also provided in the general software installer. Includes sample programs in Visual Studio.net, LabVIEW, MATLAB, LabWindows, and Keysight VEE Pro.
Programming Example 2011-05-19 |
![]() |
Binary Oscilloscope File to MATLAB Translator Program
This is a program for importing binary files from Keysight oscilloscopes into The MathWorks MATLAB.
Programming Example 2007-05-11 |
|