Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 26

Sort:
Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2018-01-18

Does M9393A work without M9300? If so, when using the M9393A with 100MHz reference on a pulse generator, what is the external reference input voltage?
When replacing the M9300 with a pulse generator, self-test and alignments may pass. Click on the question for additional information.

FAQ 2017-06-28

Is there a PDF version available of the user guide for the M9210A? There are issues with the .chm file that is available.
No, there is not a PDF version available for the M9210A user manual. To read the .chm file, it must be downloaded and copied on the local C drive before opening.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Does the M9290A CXA-m PXIe signal analyzer offer a tracking generator?
Yes, M9290A CXA-m has optional tracking generator function.

FAQ 2015-06-04

Does M9290A CXA-m PXIe Signal Analyzer support sweep mode for spectrum analysis?
Yes, the M9290A supports both sweep and FFT mode for spectrum analysis.

FAQ 2014-09-11

How do you clear the M9036A Embedded Controller memories?
Please refer to the link below for the procedure on how to clear the memories for the M9036A Embedded Controller.

FAQ 2013-04-01

How do you clear the M9045A, M9045B, M9047A and M9048A memory?
Please refer to the link below for the procedure on how to clear the memory for the M9045B and M9048A adapters.

FAQ 2012-05-01

How do you clear the M91xxA memory?

FAQ 2011-06-22

Is a dual-M9018A chassis configuration using NI PCIe-8372 connected to NI PXIe-8370 modules supported?
A dual-M9018A chassis configuration using NI PCIe-8372 and NI PXIe-8370 modules is supported...

FAQ 2011-03-08

What is the compatibility between PXIe chassis and Keysight new PXI/PXIe modules?
Keysight modules come in several varieties, so inspection is required to determine compatibility...

FAQ 2010-10-06

What is the difference between PXIe and AXIe?
The AXIe standard provides the maximum scalability to address a range of platforms...

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06

Can I replace other vendors' module (for example a digitizer) with a Keysight one?
There are two aspects to consider...

FAQ 2010-10-06

Are all PXIe system modules/controllers compatible with all chassis?
No, the PXIe standard requires the chassis support certain configurations but not all...

FAQ 2010-10-06

Does Keysight have mass interconnect solutions?
There are mass interconnect solutions from MAC panel....

FAQ 2010-10-06

Can I use SCPI to communicate with my Keysight modules?
No. Connectivity is provided through Drivers.

FAQ 2010-10-06

Will ExpressVIs work with Keysight hardware?
No. Keysight has VIs available to use with LabView but not ExpressVIs.

FAQ 2010-10-06

Can I use PXI-1 existing cards in the Keysight Card cages and are there any that will no longer work?
Older PXI (PXI-1) modules (which have a J2 present) will not work in Keysight 18-slot PXIe chassis...

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

Can I use the PXIe products over LAN?
If the PXIe chassis has an embedded controller with a LAN port then the PXI system can connect to a LAN port...

FAQ 2010-10-06

IO Libraries Suite: How do I fix the error message “Missing or Damaged GPIB-32.dll”?
Install NI-488.2 version 2.5 (or later)...

FAQ 2010-09-20

IO Libraries Suite: Is it possible to have both an NI GPIB card and a Keysight GPIB card or converter working in the same system?
Yes, it is possible with many version’s of Keysight IO Libraries.

FAQ 2010-09-08

IO Libraries Suite: Is there any other software that needs to be installed when I am using an application that utilizes NI-488.2 and Keysight IO Lib...
It depends if there is third party connectivity hardware or software installed.

FAQ 2009-08-25

1 2 Next