Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-17 of 17

Sort:
Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2018-01-18

Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

How do you clear the M9536A Embedded Controller memories?
Please refer to the link below for the procedure on how to clear the memories for the M9536A Embedded Controller.

FAQ 2013-04-01

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

How do you clear the M9045A, M9045B, M9047A and M9048A memory?
Please refer to the link below for the procedure on how to clear the memory for the M9045B and M9048A adapters.

FAQ 2012-05-01

How do you clear the M9502A and M9505A AXIe Chassis memory?

FAQ 2011-07-08

What is the difference between PXIe and AXIe?
The AXIe standard provides the maximum scalability to address a range of platforms...

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

Can AXIe LAN interface be used with all AXIe modules?
Yes. LAN (as well as PCIe) are defined by the standard but not required...

FAQ 2010-10-06

Can I use SCPI to communicate with my Keysight modules?
No. Connectivity is provided through Drivers.

FAQ 2010-10-06

Will ExpressVIs work with Keysight hardware?
No. Keysight has VIs available to use with LabView but not ExpressVIs.

FAQ 2010-10-06

What is the difference between AXIe 1.0 and 3.1?
The AXIe 1.0 specification is a base-level standard for "general-purpose" applications...

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06