検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-4 / 4

並べ替え
How do I view the streamed/recorded data from my M9203A or M9703B digitizer?
A utility is available that will convert the recorded BIN file to a data format that is compatible with Keysight's 89600 VSA Software. Click on the question above for a fuller description.

FAQ 2019-10-18

Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2018-01-18

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

What is the data transfer rate of PXI, PXIe, and AXIe?
PXI-1 has two variants...

FAQ 2010-10-06