Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

26-50 из 56

Упорядочить:
Where do I download the mechanical drawings for the Y1226A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the Y1234A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9505A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the Y1221A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9514A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9536A?
The M9536A comes with .step and .pdf files that can be imported into your modeling application.

FAQ 2014-04-01

How do I connect multiple PXIe and/or AXIe chassis together with a single controller?
PXIe and AXIe chassis can be interconnected in multiple configurations.

FAQ 2013-08-07

Why does the chassis Soft Front Panel (SFP) not start when I connect to the chassis with my Windows XP PC?
The Keysight PXIe and AXIe chassis require Microsoft .NET Framework 3.5 SP1 installed on the PC in order for the SFP to work. Windows XP does not have this loaded automatically. If you are using a Windows XP PC, please install Microsoft .NET Framework 3.5 SP1 from Microsoft website.

FAQ 2013-07-10

How do you clear the M9536A Embedded Controller memories?
Please refer to the link below for the procedure on how to clear the memories for the M9536A Embedded Controller.

FAQ 2013-04-01

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

What is the best configuration for wideband I/Q modulation?
An E8267D Option 016 or an N8212A Option 016 signal generator with an M8190A arbitrary waveform generator

FAQ 2012-12-28

Why is my M9502A or M9505A Soft Front Panel (SFP) displaying error “Unable to open instrument. Driver initialization failed.”
A 32-bit mDNS responder is required for 32-bit applications running on a 64-bit OS when using IOLS 16.2. Installing the 32-bit mDNS responder patch below will add a 32-bit mDNS responder to appropriately resolve mDNS names to an IP address for these applications.

FAQ 2012-10-10

What is the latest version of protocol software for my protocol analyzer (PCI Express, HDMI, or Fibre Channel)?
See the list of current software versions available.

FAQ 2012-08-24

How do you clear the M9045A, M9045B, M9047A and M9048A memory?
Please refer to the link below for the procedure on how to clear the memory for the M9045B and M9048A adapters.

FAQ 2012-05-01

What changed in the Fan Control for the M9502A and M9505A with firmware 1.3.23?
The Fan Speed parameter changed from 8-15 to 35-100.

FAQ 2012-03-27

Keysight Driver Migration Tool

FAQ 2012-01-20

How do you clear the M9502A and M9505A AXIe Chassis memory?

FAQ 2011-07-08

Which computers has Keysight tested with PXI or AXIe chassis?
Keysight maintains a list of tested computers...

FAQ 2011-03-14

M8190A 12 GSa/s Arbitrary Waveform Generator
March 1st question and answer session

FAQ 2011-03-07

PDF PDF 178 KB
Do these products appear in the Keysight connection expert?

FAQ 2010-10-11

What is the data transfer rate of PXI, PXIe, and AXIe?
PXI-1 has two variants...

FAQ 2010-10-06

What is the difference between PXIe and AXIe?
The AXIe standard provides the maximum scalability to address a range of platforms...

FAQ 2010-10-06

Can AXIe LAN interface be used with all AXIe modules?
Yes. LAN (as well as PCIe) are defined by the standard but not required...

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

Назад 1 2 3 Следующие