Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Type of Content

By Product Category

1-25 of 187

Sort:
MATLAB IQtools
Example MATLAB application to generate multi-tone, pulsed radar, digital modulation and high-speed serial data signals. Works in conjunction with Keysight high-speed AWGs and Vector Signal Generators.

Programming Example 2018-01-30

ZIP ZIP 3.29 MB
Get *IDN? Query Results, VISA COM library, C#
This sample program sends a *IDN? SCPI query to an instrument to get its identification string. The result is displayed on a MS Windows Console.

Programming Example 2017-04-28

ZIP ZIP 41.79 KB
Get Waveform Data, VISA COM library, VBA
This sample program gets waveform data from the oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 1.01 MB
Get *IDN? Query, Screen Image, and Waveform Data Results, VISA COM library, VBA
This sample program performs three different tasks: 1) sends a *IDN? query to the instrument and reads back the ID string, 2) captures and saves a screen image from the oscilloscope, and 3) gets the oscilloscope's waveform data from channels 1 and 2.

Programming Example 2017-04-28

ZIP ZIP 1.30 MB
Load Arbitrary Waveform Data into WaveGen, VISA library, Python
This example shows several methods for getting arbitrary waveform data into the waveform generator of a Keysight InfiniiVision X-Series oscilloscope. The oscilloscope must have the WaveGen license and support arbitrary waveforms.

Programming Example 2017-04-28

ZIP ZIP 6.08 KB
Get Screen Image and Waveform Data and Save to USB Thumb Drive, VISA library, Python
This script shows how to save a screen image and waveform data to a USB stick, with error checking.

Programming Example 2017-04-28

ZIP ZIP 5.50 KB
Get InfiniiVision Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 48.93 KB
Acquisition Synchronization, Two Simple Methods, VISA library, Python
This script shows the two best synchronization methods for all InfiniiVision and InfiniiVision X-Series oscilloscopes. Benefits and drawbacks of each method are described.

Programming Example 2017-04-28

ZIP ZIP 338.73 KB
Get Waveform Data (Elegant), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

Programming Example 2017-04-28

ZIP ZIP 13.93 KB
Get Lister Data, VISA library, Python 3.5
This script is a reference and starting point for automating Lister data capture over USB.

Programming Example 2017-04-28

ZIP ZIP 4.21 KB
Save Multiple Waveforms to a Binary File with Averaging, VEE
This sample program saves multiple waveforms to a binary file with averaging.

Programming Example 2017-04-28

ZIP ZIP 4.06 KB
Get Segmented Memory Time Tags, Waveforms, and Measurement Results, VISA library, Python
This script can get waveforms and measurements from analog channels for segmented memory already acquired on an InfiniiVision oscillocope. It can also get time tags and produce an averaged segment for each analog channel.

Programming Example 2017-04-28

ZIP ZIP 8.17 KB
Get Waveform Data, VEE
This sample program gets waveform data from the oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 4.08 KB
Get Screen Image, VISA library, Python 3.5
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

Programming Example 2017-04-28

ZIP ZIP 2.32 KB
Acquisition Synchronization, Two Simple Methods, MATLAB
This script shows how to properly initialize a Keysight InfiniiVision or InfiniiVision X-Series oscilloscope and synchronize an acquisition using the blocking :DIGitize command.

Programming Example 2017-04-28

ZIP ZIP 328.53 KB
Get Waveform Data (Brute Force), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

Programming Example 2017-04-28

ZIP ZIP 13.62 KB
Get InfiniiVision X-Series Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion X-Series oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 65.53 KB
Get Waveform Data, LabVIEW
This sample program gets waveform data from the oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 69.15 KB
Get Screen Image, VISA library, Python (2.7)
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

Programming Example 2017-04-28

ZIP ZIP 3.27 KB
Get Segmented Memory Time Tags and Measurement Results, VISA COM library, VBA
This sample program assumes the oscilloscope has been set to capture N segments. The program lists the segment number and the relative time stamp of that segment. A Delay measurement is made between channels 1 and 2 within each segment and the measurement value from each segment is listed.

Programming Example 2017-04-28

ZIP ZIP 33.08 KB
Save and Recall Setups, VISA library, Python
This script shows how to query the oscilloscope setup, save it to disk, recall it form disk, and use it to set up the oscilloscope again. This is also shown using the *LRN? query and with just trigger setups.

Programming Example 2017-04-28

ZIP ZIP 4.39 KB
Get Segmented Memory Time Tags and Measurement Results, VISA library, Python
This script figures out how many segments were acquired, flips through them, gathers the time tags and desired measurement results.

Programming Example 2017-04-28

ZIP ZIP 4.96 KB
I/O Libraries Example Programs
Examples to get you started with instrument programming...

Programming Example 2016-10-19

MIMO Config Utility 1.1.6.msi
This utility assists new users in making their first measurements when using the M9381A PXIe VSG and M9391A PXIe VSA in a MIMO environment.

Programming Example 2014-05-15

FILE FILE 737 KB
MIMO Demo Tool Install 1.2.1.msi
This demo tool provides the capability to generate multi-channel waveforms from the M9381A PXIe VSG, including waveforms and sequences of waveforms for WLAN, LTE MIMO, and Carrier Aggregation signals. This demo tool includes source code and a programming guide that can be leveraged when writing your own test code.

Programming Example 2014-05-15

FILE FILE 128.52 MB

1 2 3 4 5 6 7 8 Next