検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

絞込み

絞込みのリセット

トピック

コンテンツのタイプ

製品カテゴリ

1-25 / 39

並べ替え
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-04

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2018-01-18

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

M8000シリーズの30日間の無料試用ライセンス
M8000製品シリーズのすべての試用ライセンスへのリンクおよび概要

FAQ 2017-01-30

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How does the Microsoft end of support for Windows XP affect my M9036A?
In Keysight’s ongoing efforts and commitment to provide the best possible product quality and improve the overall customer experience with our M9036A PXIe Embedded Controller, we would like to inform you that we have made the conscious decision to not migrate the XP version of the M9036A to Windows 7.

FAQ 2014-10-12

M9290A CXA-m PXIeシグナル・アナライザは、スペクトラム解析用の掃引モードをサポートしていますか?
はい。M9290Aは、スペクトラム解析用の掃引モードとFFTモードをサポートしています。

FAQ 2014-09-11

M9036A PXIeエンベディッド・コントローラのWindows XPのサポート終了に関するガイド
2014年4月8日に、MicrosoftはWindows XPオペレーティング・システムのサポートを終了します。この日以降は、Microsoftからセキュリティ・パッチが配布されません。

FAQ 2014-04-11

[仕様] USBモジュラ型測定器は、Windows7をサポートしていますか?
はい、最新のKeysight Measurement ManagerにてWindows7 32bitをサポートしています。

FAQ 2013-06-24

GPIBインタフェース(82357A、E5810A、82350B)を使って、GPIB経由でPC上から計測器を自動計測する方法を教えてください。
GPIBインタフェース(82357A、E5810A、82350B)を使って....

FAQ 2013-06-19

How can previously created data in BenchLink II be exported?
Open a previously saved configuration file with data and then export the data as a Text (.txt) file or Comma Separated values (.csv) file.

FAQ 2012-11-05

[仕様] Keysight Measurement Managerは、Windows Vistaでサポートされていますか?
はい、Keysight Measurement Manager バージョン 1.8.3.0以上にて、Windows Vista(Service Pack 1、Business, Ultimate, Enterprise, Basic, Home Premium Editionの各種パッケージ)をサポートしています。

FAQ 2010-11-03

[仕様] Keysight Measurement Manager (AMM) は、英語以外の言語設定もサポートしますか。
はい、Keysight Measurement Manager (AMM) は、英語以外の言語設定もサポートします。

FAQ 2010-11-02

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

What drivers will be provided with modular products?
IVI-COM, IVI-C and LabVIEW (G), are provided with all Keysight modular products...

FAQ 2010-10-06

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

IO ライブラリ・スイート:サポートされているインタフェースおよびオペレーティング・システムは?
Keysight IO ライブラリ・サポート・マトリクスをご覧ください。

FAQ 2010-09-08

Why does the error message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear…
The message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear because….

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

Why do I not see all the data points on my graph tab?
When viewing your readings from the Graph Tab, some times not all of your data is displayed.

FAQ 2009-11-05

How do I avoid getting “Out of memory” exception errors when using the BenchLink DataLogger software?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

How to speed up my computer processing time while running the BenchLink DataLogger software continuously for a long period of time?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

How do I avoid getting "The memory could not be "read"" error upon closing the software?
It’s most likely this issue is caused by a bad memory...

FAQ 2009-08-19

1 2 次へ