Техническая поддержка
Электронные измерения
Уточнить список
По теме
- Calibration (1)
- Configuration & Installation (141)
- Display Messages/Error Codes (19)
- Licensing (8)
- Measurement & Instrument Fundamentals (20)
- Measurement Techniques (36)
- Operating System & Software (39)
- Operation & Functionality (171)
- Other Information (58)
- Parts & Accessories (26)
- Printing & Printers (2)
- Product & Firmware Updates & Upgrades (17)
- Product Theory of Operation (42)
- Programming & Data Transfer (81)
- Service & Maintenance (27)
- Specifications & Accuracy (38)
- Troubleshooting (17)
По типу содержания
- FAQ (664)
По типу оборудования
1-25 из 664
30 Day Free Trial Licenses for the M8000 Series
Overview of & links to all trial licenses within the M8000 product family.
FAQ 2019-11-26 |
|
Where do I download the mechanical drawings for the M9506A?
Files can be imported into your modeling application.
FAQ 2019-09-10 |
|
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.
FAQ 2019-08-28 |
|
X8711A – Help file
FAQ 2019-08-27 |
![]() |
What cable do you recommend for the M9203A I/O and Sync connectors?
Keysight cable U5300A-102, one of which is included with every M9203A order. This is 1 meter long, with MMCX (male) to BNC (male) connectors.
FAQ 2019-08-16 |
|
Does the X8711A support SCPI for remote programming?
The X8711A does not support SCPI. However, an instrument API/driver in .NET DLL is provided. Click on the link for additional information.
FAQ 2019-07-08 |
|
Where do I download the mechanical drawings for the M9037A?
Files can be imported into your modeling application.
FAQ 2019-02-01 |
|
Where Can I Find Free Trials?
Free trials of design & test software. Find free trials of the software for your product.
FAQ 2019-01-30 |
|
Where do I download the mechanical drawings for the Y1213A?
Files can be imported into your modeling application.
FAQ 2018-11-15 |
|
Where do I download the mechanical drawings for the Y1214B?
Files can be imported into your modeling application.
FAQ 2018-11-15 |
|
Where do I download the mechanical drawings for the Y1212A?
Files can be imported into your modeling application.
FAQ 2018-11-14 |
|
How do I upgrade my M9290A CXA-m PXIe Signal Analyzer?
Find Information on Hardware Options, Measurement Applications, etc....
FAQ 2018-08-13 |
|
How do I install the X8711A software?
Use the installation wizard to install the software, or see the supporting document for manual installation.
FAQ 2018-06-28 |
|
How to upgrade your Embedded Controller to Windows 10
You can easily update your Embedded Controller to Windows 10 by swapping out the SSD with a new Windows 10 SSD.
FAQ 2018-06-07 |
|
Where can I get a good study tool to teach me about the Keysight PXIe chassis?
Please download the PXI Chassis Interactive Block Diagram and view it using Adobe Acrobat.
FAQ 2018-05-31 |
|
What are the Memory Information and Procedures of the E8404A ?
FAQ 2018-04-19 |
|
How Do I Measure the Bit Error Rate (BER) to a Given Confidence Level on the J-BERT M8020A and the M8040A High-Performance BERT?
How do I measure Bit Error Rate (BER) to a given confidence level on J-BERT M8020A and M8040A high-performance BERT?
FAQ 2018-03-01 |
|
IO Libraries Suite: What is the latest version? IO Libraries Suite 2018 Update 0.2
IO Libraries Suite 2018 Update 0.2, available online.
FAQ 2018-01-31 |
|
Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.
FAQ 2018-01-18 |
|
What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.
FAQ 2018-01-18 |
|
M8020AU Upgrades for J-BERT M8020A high-performance BERT
M8020A/M8040A Post Purchase Upgrade Option
FAQ 2017-12-13 |
|
Signal Analyzer LabVIEW Instrument Drivers
Supported models: N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, N8973B, N8974B, N8975B, N8976B, M8920A
FAQ 2017-12-01 |
|
What is the Embedded Controller Default Password? Answer: Keysight4u!
The default password is “Keysight4u!” for the Administrator account for Windows 10 Enterprise 2016 LTSB. We recommend that you change the password for improved security, because the default password is public knowledge.
FAQ 2017-11-14 |
|
Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF.
Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states.
If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly.
To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF.
Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.
FAQ 2017-11-13 |
|
Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA
FAQ 2017-09-21 |
|