Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По типу содержания

1-25 из 29

Упорядочить:
Keysight, UC San Diego Demonstrate the World's Fastest 28 GHz 5G Band, Bidirectional Phased-Array
Record-setting 8 Gbps data rate achieved using bidirectional 64-element link with phased-array beam-pointing capabilities—supports applications in 5G, aerospace and defense

Материалы для прессы 2017-06-05

Keysight Technologies Introduces Scalable PXI Microwave Signal Generator
New PXIe signal generator meets critical 1 percent EVM and 1 GHz bandwidth requirements for complex waveforms up to 44 GHz

Материалы для прессы 2017-06-05

New PXIe Instruments for 5G, A&D and Quantum Technologies
New PXIe Instruments for 5G, A&D and Quantum Technologies

Материалы для прессы 2017-05-31

Three new PXle Chassis - from low-cost to high-performance

Материалы для прессы 2017-02-22

Keysight Technologies Expands the M8000 Series for 400 GbE
New 64 GBaud BERT Simplifies Accurate Characterization of PAM-4 and NRZ Devices

Материалы для прессы 2016-07-25

Keysight Technologies Expands its M8000 Series of BER Test Solutions for Multi-Channel Applications
Keysight Technologies introduced a multi-channel BERT solution based on a 14-slot AXIe mainframe for multi-lane testing. The BERT uses the latest version of the M8070A system software, version 3.0. The M8000 series of BER test solutions provide faster insight into multi-channel applications.

Материалы для прессы 2016-06-10

Keysight Technologies Expands the M8000 Series for 400 GbE - Press Release
Keysight Technologies, Inc. introduced a M8040A high-performance BERT for testing PAM-4 and NRZ devices that operate up to 64 GBaud. Engineers in validation labs and R&D who characterize receivers on the physical layer for the next generation of data center interconnects will benefit from simplified test setups and repeatable and accurate results.

Материалы для прессы 2016-05-18

Keysight Technologies Introduces MIPI® Receiver Test Software for PHY-Layer Standards
New Software Enables Automated Testing According to Conformance Test Suite for MIPI C-PHY 1.0 Standard

Материалы для прессы 2015-10-26

Keysight Technologies Introduces Industry’s Highest Performance PXIe Multiport Vector Network Analyz

Материалы для прессы 2015-09-22

Keysight press release at ECOC, Valencia, September 2015
Keysight press release at ECOC, Valencia, September 2015

Материалы для прессы 2015-09-17

Keysight press release on introduction of new arbitrary waveform generator M8196A, September 2015
Keysight press release on introduction of new arbitrary waveform generator M8196A, September 2015

Материалы для прессы 2015-09-17

Keysight Technologies to Show New Test and Measurement Solutions at ECOC 2015
Keysight's new solutions are intended to enable the development of next-generation networks used for the generation and analysis of coherent optical modulated signals. These solutions will address new modulations techniques such as PAM-4, the characterization of electrical and optical transceivers, and component test.

Материалы для прессы 2015-09-15

Keysight Technologies Introduces Industry's First Modular Stimulus Response Measurement Solution

Материалы для прессы 2015-07-01

Keysight Technologies’ PXI VNA Wins Multiple Industry Awards

Материалы для прессы 2015-04-02

Highly Integrated J-BERT Simplifies Testing for Next-Generation Data-Center, Long-Haul-Communication
Highly Integrated J-BERT Simplifies Testing for Next-Generation Data-Center, Long-Haul-Communication Applications

Материалы для прессы 2015-03-24

PLTS 2015 Reduces Multiport Fixture Removal and Associated Error-Correction Time by 75 Percent

Материалы для прессы 2015-03-02

PLTS Software 2015 Reduces Multiport Fixture Removal & Associated Error-Correction Time by 75%
Keysight Technologies’ Physical Layer Test System Software 2015 Reduces Multiport Fixture Removal and Associated Error-Correction Time by 75 Percent

Материалы для прессы 2015-01-28

J-BERT offers adjustable and integrated inter-symbol interference
J-BERT offers adjustable and integrated inter-symbol interference

Материалы для прессы 2015-01-22

Keysight Introduces Industry's First PXIe Signal Analyzer to Provide Swept & FFT Capabilities

Материалы для прессы 2014-09-16

Keysight Technologies' New, Full Two-port 26.5 GHz Vector Network Analyzers Fit in Just One PXI Slot

Материалы для прессы 2014-09-15

M8195A 65GSa/s AWG – Press Release
Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator

Материалы для прессы 2014-09-10

Introduces Industry's Most Accurate Test Solution for USB 3.1 Receivers
Achieve accurate receiver characterization with the J-BERT high-performance BERT

Материалы для прессы 2014-07-09

Press Releases for M8000 Series
New M8000 Series of BER Test Solutions

Материалы для прессы 2014-03-18

Press Releases for M8190A

Материалы для прессы 2013-09-06

Press Release for M8192A
Infinite Playtime and Multichannel Support introduced for Arbitrary Waveform Generator

Материалы для прессы 2013-09-05

1 2 Следующие