検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-9 / 9

並べ替え
Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Can I use the triaxial cable with B2900A?
Yes. You can use the triaxial cable by using the N1294A adaptor.

FAQ 2012-11-20

How Do I Find My Host Information?
The Host ID is the model and/or serial number of the product, both of which can be found on the serial number label on the back of the instrument.

FAQ 2012-06-14

What kind of interface can I use to control the B2900A?
The GPIB, USB and LAN are available to control the B2900A.

FAQ 2011-05-18

Why USB modular instruments (U272XA, U2741A, U2751A and U2761A) is not detectable by E5813A?
PC is failed to enumerate the USB modular instrument.

FAQ 2010-04-09

Is U2722A compatible with E5813A?
No

FAQ 2010-03-22

Is U2723A compatible with E5813A?
No

FAQ 2010-03-22

N6751AおよびN6752AモジュールのLGAオプションの内容は?
LGAオプションは、N6751A/52Aモジュールに対して強く推奨されます。

FAQ 2009-12-20