这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

技术支持

自动 X 射线检测 [已停产]

按产品型号支持:

76-100 / 119

排序:
One Billion Solder Joints and Counting
Written by Stig Oresjo, Agilent Technologies. Published with permission from Circuits Assembly, February 2001.

文章 2003-02-01

PDF PDF 1.81 MB
When to Use AOI, When to Use AXI, and When to Use Both
by Stig Oresjo, senior test strategy consultant at Keysight Technologies.

应用说明 2002-12-01

PDF PDF 70 KB
Interactive Board Complexity Calculator
Calculate Your Board's Complexity Index.

应用说明 2002-11-01

Memory Specifications for 5DX Software Releases
All Keysight 5DX System Controllers and TDWs prior to the Series 3 will require a memory upgrade prior to loading software version 8.0.

用户手册 2002-10-24

Preparing a .cc File for Export to Test Link
This procedure describes the process of converting ECAD data into a form that can be used by Test Link.

应用说明 2002-10-16

PDF PDF 70 KB
Foundations for Intelligent Testing
Electronic products are becoming more complex. Lofty speeds and circuit densities unimaginable just a few years ago have become commonplace, and the trend shows no signs of abating.

技术总览 2002-10-15

5DX Series 5000 Site Preparation Manual
This document describes what needs to be done prior to the 5DX system delivery.

安装手册 2002-10-01

PDF PDF 584 KB
Remote Network Connections Creation for the Operator Logon
Operator logon on the Keysight 5DX Series II System is limited, in that it does not allow Operator to make network connections that are required for sending images and res files to the PLR workstation.

应用说明 2002-06-30

AwareTest xi Product Demonstration
A Demonstration of Aware Test xi... an intelligent test solution for testing high-complexity boards.

基本演示 2002-06-15

Using NDFCOL.EXE, the NDF "Line Up the Columns" Utility
NDFCOL.EXE is a handy little utility that will form neat columns of data in NDF files.

应用说明 2002-06-06

Charting a DFT Course for Limited Access Boards
Written by Stig Oresjo and Barry Odbert. Published with permission from SMT Magazine, June 2002.

文章 2002-06-01

PDF PDF 143 KB
Obtaining a Listing of Applications on Series II Systems
There is currently no easy way to obtain a list of all resident applications on a 5DX System or TDW. It is difficult to match panel name with hash name and see when the application was last updated.

应用说明 2002-06-01

Sampling on the Keysight 5DX
Sampling Mode allows test coverage to be optimized with line speed. This document explore the setup procedure for the Keysight 5DX for sampling.

应用说明 2002-05-08

AwareTest xi Software Profile
Keysight AwareTest xi software allows Keysight 5DX and Keysight 3070 test systems to collaborate intelligently for shorter test cycles.

产品资料 2002-04-29

PDF PDF 933 KB
5DX Series 5000 Installation Guide
This document is intended to guide you through the Keysight 5DX installation process.

安装手册 2002-04-01

PDF PDF 1.52 MB
Memory Upgrade Procedures for 5DX Software Releases
These documents detail the specific memory modules needed for 5DX System Controllers.

用户手册 2002-01-01

AwareTest xi Process Guide
Process guide for the AwareTest xi software solution.

用户手册 2001-11-01

PDF PDF 1019 KB
The Life of a 5DX Inspection C# File
The {Hashed Panel Name}.C# file is basically cad information about a panel program. It is used in conjunction with various utilities to overlay cad data on images or provide cad data for filters.

应用说明 2001-10-16

PDF PDF 97 KB
Comparing AOI and AXI
Choosing the right technology requires looking at board mix, capital budget and other business considerations. But most of all, you need to understand the typical characteristics of each technology.

应用说明 2001-07-25

PDF PDF 42 KB
Version 7.x ASAP Best Practices
In an effort to standardize programming practices for the Keysight 5DX, Keysight has created a set of procedures representing 5DX "best practices" that address various aspects of the programming process.

应用说明 2001-07-25

Taking and Using Diagnostic Images
Storing images can be a helpful method for trouble-shooting and collaboration with support. This document explains the methods for taking images. In addition to the software revisions named, the document applies to all 5DX software versions.

应用说明 2001-05-17

PDF PDF 61 KB
Rotating Boards on a Panel
Rotating Boards on a Panel if often necessary. In addition to the software revisions named within, the explained technique in the document is utilized for for 4.x, 5.x, 6.x and 7.x. For 8.x Test Link deals with this automatically.

应用说明 2001-05-17

PDF PDF 40 KB
Series II Compliance with the Machinery Directive (in Europe) - specific installation procedures
Series II will meet requirements of Machinery Directive in European Community member countries, if the following steps, which are described in the document, are taken during installation of equipment.

应用说明 2001-05-17

Dealing with Board Thickness Variations
The Keysight 5DX has the capability to be implemented such that it can accommodate thickness variations on a board-by-board basis. NOTE: Content described is in the 5DX Reference Guide but is no longer in Chapter 7 as mentioned herein.

应用说明 2001-05-16

PDF PDF 31 KB
5DX Series 3 Installation Guide
This document is intended to guide you through the Keysight 5DX installation process.

安装手册 2001-05-01

PDF PDF 1.40 MB

以前 1 2 3 4 5 下一页