这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

技术支持

自动 X 射线检测 [已停产]

按产品型号支持:

1-25 / 73

排序:
5DX Windows 7 Controller Upgrade - Flyer
Upgrade your 5DX AXI PC controller to enjoy better inspection performance.

手册 2017-12-01

PDF PDF 547 KB
Automated X-Ray Inspection System Keysight Technologies - Technical Overview
This is a technical datasheet. Keysight has developed a sealed ultra-high vacumn X-ray tube that provides stable output throughout a significantly long life.

技术总览 2015-03-24

PDF PDF 644 KB
Maximize Your Keysight AXI Coverage with Flexible Pricing - Brochure
This flyer describes the different support options Keysight AXI users can select from to ensure peace of mind for covering the support needs of their 5DX and x6000 investments.

手册 2014-07-31

PDF PDF 141 KB
Ball Grid Array Joint Inspection Using X-ray as it relates to voids and the IPC-7095A specification
With the introduction of Lead-free solder, voiding within Ball Grid Array (BGA) joints is potentially a major issue. This article discusses the relationship to voiding, the IPC standard and Automated X-ray Inspection.

专访 2012-12-06

PDF PDF 105 KB
Diagnostic Testing and the Medalist 5DX Automated X-ray Inspection System
Users of the Medalist 5DX automated x-ray inspection system can benefit from running diagnostic tests on a regular basis. This application note provides some guidelines.

应用说明 2009-01-14

PDF PDF 188 KB
Successful Implementation of the Keysight Medalist x6000 AXI Solution – The Pyramid Concept
This aplication note provides a pyramid concept that outlines how users can successfully leverage the powerful defects detection capabilities of the Keysight Medalist x6000 automated x-ray inspection system to reduce their production and life cycle costs and improve product quality.

应用说明 2008-11-19

PDF PDF 55 KB
Exposed Pad Algorithm for the Medalist x6000 AXI System
This application note describes how to use the exposed pad algorithm in the Medalist x6000 AXI software to test all varieties of QFN and FET package types for defects such as Open and Voiding.

应用说明 2008-10-21

PDF PDF 1.83 MB
Setting Up HotKeys for AXI products on the Keysight Medalist Repair Tool
Users of the Keysight Medalist Repair Tool, also known as the Keysight Repair Tool (ART), can setup hot keys to increase the efficiency of image viewing in RT4.0 for their X-ray inspection products.

应用说明 2008-09-26

PDF PDF 629 KB
codeNexus - Defect Reporter
Defect Reporter enchancement for the Medalist 5DX Automated X-ray Inspection System

应用说明 2008-09-26

PDF PDF 764 KB
Build Operator Menu: Multiple Menu Configuration Control for 5DX Auto User Interface
The "Build Operator Menu" software replaces and extends the functionality found in the BLDOPMNU DOS command. This application note provides useful user information about this menu.

应用说明 2008-09-04

PDF PDF 849 KB
Adjusting the X-ray Surface Map parameters on the Medalist 5DX Automated X-ray System
Tips on obtaining the best images using the 5DX surface map parameters.

应用说明 2008-08-27

Quad Flat No Lead (QFN) Best Practices
The purpose of this application note and best practices guide is to describer the QFN-type component and provide testing methods to ensure robust testing on the Medalist 5DX Automated X-ray Inspection (AXI) System.

应用说明 2008-08-26

PDF PDF 492 KB
Keysight 5DX 8.50 Software Release
The Keysight Technologies Automated X-ray Inspection System 8.50 software release for the 5DX is available.

发布说明 2008-08-21

Using the FET Algorithm on the Medalist 5DX AXI to Analyze Non-Standard Joints
A new algorithm family called FET for the Keysight Medalist 5DX automated X-ray inspection (AXI) system helps users to effectively analyze non-standard joints for insufficient or no solder, non-reflowed or cold solder, and excessive voiding.

应用说明 2008-07-01

PDF PDF 553 KB
Adjusting the Defect Analyzer detection parameters on the Medalist 5DX Automated X-ray System
Defect Analyzer operates by making a small change in the ‘z’ height of the board and re-testing suspect joints.

应用说明 2008-06-12

Keysight 5DX 操作手册
该操作手册描述 5DX 的安全性和操作流程。

运行手册 2008-06-01

Results from 2007 Industry Defect Level and Test Effectiveness Studies
To select an optimal test strategy, good knowledge of defect levels and test effectiveness are two very important factors to include. This paper presents data from a 2007 study of 3.7 billion solder joints. Reprinted with permission from IPC.

文章 2008-05-21

PDF PDF 118 KB
Article reprint: Impact of Quad Flat No Lead Package (QFN) on Automated X-ray Inspection (AXI)
This paper discusses lack of industry specification for QFN inspection, how AXI methodology was improved to detect QFN solder joint defect, design for inspection and future work.

文章 2008-03-06

PDF PDF 1.63 MB
How CAD Data and Threshold Settings Affect Pin Length on the Keysight Medalist 5DX
This application note describes the effects of CAD data and threshold settings on pin lengths while working on the Medalist 5DX Automated X-Ray Inspection system.

应用说明 2008-02-22

PDF PDF 124 KB
Comparing CAD and BOM data for 5DX Use
Instructions for comparing CAD and BOM data to quickly deal with no load components.

应用说明 2008-01-04

PDF PDF 1.16 MB
Keysight x6000 操作手册
该操作手册描述 x6000 的安全性和操作流程。

运行手册 2007-12-01

Xray Choices for SMT Manufacturing
In many cases, there is a complementary choice of automated 3D X-ray and off-axis 2D X-ray inspection. This article explores this concept. Published with kind permission from SMT

文章 2007-11-01

PDF PDF 188 KB
Tips for X-ray Users On Exporting NDF’s With No Loads Set To False
Navigating CAD can be a time consuming process. Small tips can be extremely helpful in creating quality programs in a short amount of time.

应用说明 2007-10-18

X-ray Test Users Utilize BOM Explorer to Change
Automated X-ray Inspection 5DX Users can save time by implementing these quick and easy steps to use BOM explorer to change "no pops" to "untested".

应用说明 2007-10-12

Carrier Usage with the x6000 Automated X-ray Inspection System
Carriers can be used successfully in the x6000 Automated X-ray Inspection system. Several factors need to be considered when designing a carrier. This document outline the factors that should be considered in the carrier design.

应用说明 2007-08-23

1 2 3 下一页