这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-21 / 21

排序:
How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

ENA 支持什么机械校准套件和电子校准件?
请参见下面的文档……

FAQ 2012-12-11

针对 Keysight ENA 系列矢量网络分析仪,建议使用哪种运输箱?
目前还没有针对 ENA 和 ENA-L 系列而专门定制的运输箱。不过,是德的 9211-2658 运输箱足以容纳一台 ENA-A、ENA-B、ENA-C 或 ENA-L 系列矢量网络分析仪。

FAQ 2012-02-28

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

ENA 是否包括具有使用年限的部件?
是。

FAQ 2011-10-07

85039B F型校准套件的延迟/直通定义值是否有错误?
定义值没有错误,但测量可插入的被测件时必须修改定义值。

FAQ 2011-10-07

85033E 30kHz至9GHz校准套件中的适配器是不是相位匹配的?
是。

FAQ 2011-10-07

如何为是德产品找到附件?
对于特定仪器附件(例如,用于示波器的探头),您首先应该访问产品页面,然后再查阅相关附件。 对于通用附件(例如,射频和微波测试)

FAQ 2011-10-07

What is the possible cause of the difference when the permittivity measured with the 16453A is different from the value previously obtained?
Most likely cause of the measurement discrepancy or drift is insufficient electrode pressure due to improper pressure adjustment.

FAQ 2011-06-07

What is the interface cable or adapter required to control external GPIB equipment by using VBA macro function of the E4991A?
The 10833A/B/C/D, 82357A or 82357B is required depending on the OS version of the E4991A.

FAQ 2011-06-07

Why is permeability measurement result unstable when a low permeability magnetic material or a thin magnetic material is measured with the 16454A?
It is because the impedance of the magnetic material inserted into the 16454A is too low for the impedance analyzer to measure it accurately.

FAQ 2011-06-07

Can the 42941A probe be used with any RF test fixture adapter?
No, the 42941A does not have any test fixture adapter available for connecting the probe to an RF component test fixture.

FAQ 2011-06-07

Can the 42941A probe be substituted for discontinued 41941A/B probe?
No, the 42941A cannot be substituted for the discontinued 41941A/B and doesn’t have compatibility with old 4194A analyzer.

FAQ 2011-06-07

How should a DC blocking capacitor be inserted between the 42941A probe and a DUT when a live DC voltage exists on the device?
It is recommended to insert a SMA DC blocking adapter between the furnished pin probe and 3.5-mm connector at the tip of the 42941A.

FAQ 2011-06-07

如何订购 Keysight 42941A 阻抗探头的替换探针?
订购部件编号为 42941-60004 的是德产品

FAQ 2010-03-16

How can I order 10 µF Standard Capacitor to retrofit the 16380C with Option 001?
The 16380V-001 Upgrade Kit for adding 10 µF capacitor is available.

FAQ 2009-07-07

The key cap of the power switch tends to come unfastened. What measure can I take to meet the situation?
It is recommended to replace with 0371-3953.

FAQ 2008-06-30

Would you give me the information on part number changes for the mechanical parts?
Please refer to the following table.

FAQ 2008-06-29

What is the part number of the GPIB I/F?
Parts number is E4970-66533.

FAQ 2008-06-27

Why does the probe pin bend a little?
The bend prevents the pin hall.

FAQ 2008-06-27

What are the default calibration kit selections on the 4395A and 4396B Combination Analyzers?

FAQ 2007-03-27