这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 30

排序:
Drive Down the Cost of Test Using the ENA Series Vector Network Analyzers - Application Note
Discussion of the contributions of the Keysight ENA series vector network analyzer to drive down the cost of test in production lines. Including an in depth analysis of the total cost of ownership.

应用说明 2019-06-04

PDF PDF 2.42 MB
Power of Impedance Analyzer - Application Note
This application note describes the necessity of real-characteristics evaluation, and shows that the impedance analyzers only have capabilities to achieve real-characteristics.

应用说明 2019-01-28

Performing Impedance Analysis with the E5061B ENA Vector Network Analyzer - Application Note
This application note describes five common impedance analysis approaches used with impedance analyzers and network analyzers. It also describes how and when to use the E5061B for impedance analysis.

应用说明 2018-03-02

PDF PDF 2.10 MB
Impedance Analyzers and Network Analyzers - Application Note
This application note describes the benefits of using USB and LAN interfaces compared to GPIB. The target instruments are bench-top network analyzers, impedance analyzers and LCR meters.

应用说明 2018-01-18

使用 Keysight E5061B 低频 — 射频网络分析仪 测量频率响应
使用 Keysight E5061B 低频 — 射频网络分析仪 测量频率响应

应用说明 2017-11-27

是德科技 使用网络分析仪进行时域分析
是德科技 使用网络分析仪进行时域分析

应用说明 2017-11-27

是德科技 使用网络和阻抗分析仪评测 13.56 MHz RFID 标签和 阅读器/记录器
是德科技 使用网络和阻抗分析仪评测 13.56 MHz RFID 标签和 阅读器/记录器

应用说明 2017-11-27

是德科技 使用 LCR 表和阻抗分析仪测量介电常数和 导磁率的解决方案
是德科技 使用 LCR 表和阻抗分析仪测量介电常数和 导磁率的解决方案

应用说明 2017-11-26

是德科技利用Keysight ENA 系列网络分析仪进行无线充电(WPT)测量
是德科技利用Keysight ENA 系列网络分析仪进行无线充电(WPT)测量

应用说明 2017-11-24

是德科技使用 E5061B 低频-射频网络分析仪测量直流-直流转换器和 PDN
是德科技使用 E5061B 低频-射频网络分析仪测量直流-直流转换器和 PDN

应用说明 2017-11-23

Impedance Measurement Handbook - 6th Edition - Application Note
This 140 page handbook is Keysight Technologies's most detailed information on the basics of impedance measurements using Keysight's LCR meters and impedance analysers. It provides the theory, test set-upinformation, error discussion, etc.

应用说明 2016-11-02

E5080A ENA 系列网络分析仪
E5080A ENA 系列网络分析仪

应用说明 2015-06-25

Materials Measurement: Soil Materials - Application Brief
Soil materials such as rocks or clay also have electrical properties in addition to the mechanical properties as with other substances.

应用说明 2014-11-05

PDF PDF 925 KB
Materials Measurement: Liquid Materials - Application Brief
This application brief provides the solutions for measuring dielectric properties of liquid materials.

应用说明 2014-08-04

PDF PDF 1.24 MB
Materials Measurement: Dielectric Materials - Application Brief
This application brief provides the solutions for measuring dielectric materials.

应用说明 2014-07-17

PDF PDF 935 KB
Materials Measurement: Magnetic Materials - Application Brief
This application brief provides the solutions for measuring magnetic materials.

应用说明 2014-07-17

PDF PDF 1.08 MB
E4990A Impedance Analyzer Migration Guide from 4294A
This migration guide describes the difference between the E4990A and 4294A impedance analyzers.

应用说明 2014-06-15

XLS XLS 40 KB
Impedance and Network Analysis Application List Application Note
This document provides the information of unique and new solutions for impedance and network analysis with using Keysight impedance analyzers, LCR meters and ENA series network analyzers.

应用说明 2012-10-30

是德成功测量阻抗的 8 点提示 应用指南 346-4
是德成功测量阻抗的 8 点提示 应用指南 346-4。测量阻抗有几种不同的技术和方法,应该根据测量的频率范围、要测量的阻抗参数以及想要显示的测量结果来选择一个具体的测试技术。

应用说明 2011-12-31

Design Tutorial: E5061B ENA Custom Multiport Switch Solution Using L4491A
This application note describes how to configure a 12-port custom switch box with the L4491A switch platform and operation basics using the E5061B network analyzer.

应用说明 2011-11-29

PDF PDF 1016 KB
New Technologies for Accurate Impedance Measurement (40Hz to 110MHz)
Auto-balancing bridge method is the best technique to make an accurate impedance measurement in LF frequency. The recent technical innovation successfully expanded its upper frequency limitation from 40MHz to 110MHz. This Product Note discusses how its made and other new technologies included in...

应用说明 2008-11-20

Balanced Circuit Measurement with an Impedance Analyzer/LCR Meter/Network Analyzer (AN 346-2)
This application note describes the difference between a balanced circuit and an unbalanced circuit, and also explains how to make an unbalanced circuit measurement by the unbalanced instrument step by step.

应用说明 2008-04-10

PDF PDF 116 KB
16196A/B/C/D Correlating RF Impedance Measurements When Using SMD Test Fixtures
This Product Note explains that the ability to verify the correlation of impedance measurement results is dependent on the variety of factors.

应用说明 2007-03-06

Temperature Characteristic Evaluations of RF Components and Materials (AN 1464)
This application note introduces an efficient and highly reliable measurement system for evaluating temperature characteristics of components and materials using a combination of the E4991A-007.

应用说明 2004-10-14

Evaluation of MOS Capacitor Gate Oxide C-V Characteristics Using the Keysight 4294A(PN4294-3)
As a result of extremely high integration of logic LSIs, MOS FETs with gate lengths of 0.1 mm or less have been produced recently. A consequence of this miniaturization has been the need for very thin gate oxide layers.

应用说明 2003-06-26

1 2 下一页