这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 50

排序:
How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

How can the E4980A or the 4263B measure internal impedance of batteries?
Insert DC blocking capacitors between the measurement terminals and a battery DUT. The 16065C can substitute for the DC blocking capacitors.

FAQ 2011-06-07

What is the possible cause of the difference when the permittivity measured with the 16453A is different from the value previously obtained?
Most likely cause of the measurement discrepancy or drift is insufficient electrode pressure due to improper pressure adjustment.

FAQ 2011-06-07

Why is permeability measurement result unstable when a low permeability magnetic material or a thin magnetic material is measured with the 16454A?
It is because the impedance of the magnetic material inserted into the 16454A is too low for the impedance analyzer to measure it accurately.

FAQ 2011-06-07

Can the 16338A be used with LCR meters such as the 4263B and the E4980A?
No, the 16338A Test Lead Set doesn’t have compatibility with LCR meters. The 16338A can be used with the 4338A/B only.

FAQ 2011-06-07

Can the 42941A probe be used with any RF test fixture adapter?
No, the 42941A does not have any test fixture adapter available for connecting the probe to an RF component test fixture.

FAQ 2011-06-07

Can the 42941A probe be substituted for discontinued 41941A/B probe?
No, the 42941A cannot be substituted for the discontinued 41941A/B and doesn’t have compatibility with old 4194A analyzer.

FAQ 2011-06-07

How should a DC blocking capacitor be inserted between the 42941A probe and a DUT when a live DC voltage exists on the device?
It is recommended to insert a SMA DC blocking adapter between the furnished pin probe and 3.5-mm connector at the tip of the 42941A.

FAQ 2011-06-07

Can the cylindrical insulator reduce the effect of magnetic coupling between the inductive DUT and the outer conductor of the 16196A/B/C/D fixtures...
Yes, but the effect of reducing the magnetic coupling effect is not sufficient and depends on the DUT.

FAQ 2010-07-02

How can I connect a test fixture to the measurement terminals of the E4980A when the stopper at the rear of the fixture disturbs the connection?
Remove the stopper from the test fixture by removing a screw at the center of the plastic stopper. Otherwise, remove the front rubber guide from the E4980A.

FAQ 2010-07-02

Do the coaxial Short and 50 Ω Load terminations for the 42941A have accuracy specifications?
No, both the coaxial Short and 50 Ω Load standard terminations for the 42941A do not have accuracy specifications.

FAQ 2010-07-02

Is there any effective way to measure the impedance of a pressure sensitive SMD component (ex. a ferrite bead) with the 16196 series or 16197A test...
In order to measure a pressure sensitive device, the pressure applied to the DUT by the test fixture needs to be carefully controlled.

FAQ 2010-07-02

在不使用 16453A 和 16454A 的情况下,E4991A 选件 002 是否可以测量电容率或导磁率?
否,使用 E4991A 选件 002 测量电容率或导磁率时,必须使用 16453A 或 16454A。

FAQ 2010-05-24

为什么总是在 16190B 空气管线中心导体的一侧刷上黑漆?
刷上黑漆标记是为了标明连接到测试端口的中心导体的方向。

FAQ 2010-05-24

When fabricating a custom test fixture for the Keysight 4339B, what are the recommendations to extend the measurement and interlock cables?

FAQ 2010-05-11

如何订购 Keysight 42941A 阻抗探头的替换探针?
订购部件编号为 42941-60004 的是德产品

FAQ 2010-03-16

16047A 与 16047D 之间存在哪些差异?

FAQ 2009-08-13

How can I order 10 µF Standard Capacitor to retrofit the 16380C with Option 001?
The 16380V-001 Upgrade Kit for adding 10 µF capacitor is available.

FAQ 2009-07-07

16092A夹具是否可与4395A/4396B/4287A分析仪一起使用?

FAQ 2009-01-14

How can I replace the contact electrodes of the 16118A?
The contact electrodes of the 16118A cannot be replaced by user.

FAQ 2009-01-13

What are the differences between the 16048A and the 16048D?
The differences between the 16048A and 16048D are shown in the table below...

FAQ 2009-01-13

How can I get a 0603 size LOAD standard that can be used to perform LOAD correction using the 16196C and other SMD test fixtures?
Keysight part number 0699-6926 can be used as a LOAD standard. It is a 51-ohm chip resistor.

FAQ 2009-01-13

What is the purpose of the grounding lead of the 16048D?
The grounding lead of the 16048D is used to interconnect this shielding conductor and the ground terminal on LCR meter's front panel.

FAQ 2009-01-13

当使用SMD夹具时,影响阻抗测量相关性的因素有哪些?

FAQ 2009-01-13

Isn't the current 16034E equipped with a dual-post stopper while previous ones had the stopper attached to the right side of Hcur connector?
The 16034E currently has no stopper because all impedance analyzers that required the stopper became obsolescence by 2001.

FAQ 2009-01-13

1 2 下一页