Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-9 из 9

Упорядочить:
Why is the "E-230 data corrupt or stale" error message occasionally displayed on the E4980A while saving a measurement data in the USB memory stick...
It is caused when the procedure for saving a data is not performed correctly or when the USB memory stick is not compatible with the E4980A.

FAQ 2011-07-24

Why does the 42841A shut down with an error message display on the E4980A/ 4284A when DC bias current exceeds a certain level?
The 42841A cannot output DC bias current in excess of a level determined from the DC resistance of DUT and the maximum limit of DC output voltage.

FAQ 2011-04-21

Can the E4980A/ 4284A measure DUT when "Warning, ALC unable to regulate" is displayed?
Yes, the E4980A/ 4284A can measure DUT though the test signal level is not controlled at the ALC setting value.

FAQ 2010-01-26

How can I check for anomaly in test fixture when the E4980A/ 4263B/ 4284A/ E4981A fails in open/short compensation for a particular test fixture?

FAQ 2010-01-26

When the E4980A/4284A LCR meter displays "ALC unable to regulate" error message, what corrective action should be performed?

FAQ 2009-08-13

Why does the E4980A display OVERLOAD when DC bias current setting is above 20 mA?
If the DCI range has been set to 20 mA (default setting), change it to AUTO or 100 mA range.

FAQ 2008-11-12

How does the E4980A operate when the USB stick memory overflowed?
The E4980A doesn't store new data into the USB memory.

FAQ 2008-06-12

How does the E4980A operate when the buffer memory overflowed?
The E4980A doesn’t store the subsequent data into the buffer memory.

FAQ 2008-06-12

How can I clear the data buffer memory of the E4980A when an error message "E90: Data buffer overflow" appears?
Use :MEM:CLE DBUF command or press "SAVE & STOP" softkey.

FAQ 2008-06-12