这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-19 / 19

排序:
E4980A 和 42841A 之间的电缆的部件编号(P/N)是什么?
最新的电缆部件编号为 E4980-61640。

FAQ 2014-02-06

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

当在USB 闪存中保存测量数据时,为什么 E4980A 上偶尔会显示“E-230 数据损坏或失效”的错误消息?
当未能正确执行保存数据的程序时,或者当 USB 闪存不兼容 E4980A 时,便会出现以上情况。

FAQ 2011-07-24

哪种 USB 存储器件适用于 E4980A 和 E4981A?
建议使用 4 GB USB 存储器(Keysight PN 1819-0637)。

FAQ 2011-07-11

How can the E4980A or the 4263B measure internal impedance of batteries?
Insert DC blocking capacitors between the measurement terminals and a battery DUT. The 16065C can substitute for the DC blocking capacitors.

FAQ 2011-06-07

Can the 16338A be used with LCR meters such as the 4263B and the E4980A?
No, the 16338A Test Lead Set doesn’t have compatibility with LCR meters. The 16338A can be used with the 4338A/B only.

FAQ 2011-06-07

How can I connect a test fixture to the measurement terminals of the E4980A when the stopper at the rear of the fixture disturbs the connection?
Remove the stopper from the test fixture by removing a screw at the center of the plastic stopper. Otherwise, remove the front rubber guide from the E4980A.

FAQ 2010-07-02

如何订购 4285A 选件 201、202 和选件 301 的操作指南?
4285A 选件 201/202 处理器接口和选件 301 扫描仪接口的操作指南列在 4285A 操作手册(序列号 04285-90010)结尾部分的附录中。

FAQ 2009-08-13

How can I order 10 µF Standard Capacitor to retrofit the 16380C with Option 001?
The 16380V-001 Upgrade Kit for adding 10 µF capacitor is available.

FAQ 2009-07-07

Is there a 16060A-like transformer test fixture usable with the E4980A?
No transformer test fixture for the E4980A is available.

FAQ 2009-03-11

Can I use the 16048B with the 4285A for the cable extension?
Yes, the 16048B (Part Number 16048-60030) can be used with the 4285A. But, it is not easy to perform the cable correction using the 100-ohm resistor box (furnished with the 4285A).

FAQ 2009-01-13

What compensation should I perform when I use the 16048B with the 4285A?
It is recommended to set the Cable Length function of the 4285A to "1 m" and perform open/short/load compensation at the DUT contact terminals of the test fixture connected to the tip of the 16048B.

FAQ 2009-01-13

What is the part number of pull-up resistors recommended for the option E4980A-201 handler I/F of the E4980A?
Recommended resistance values and part numbers of the pull-up resistors are shown in the following table.

FAQ 2008-11-12

Is there any ID to discriminate incompatible USB memory from E4980A compatible ones?
See the following ID of incompatible USB memory devices.

FAQ 2008-11-12

Is the E4980A compatible with all the test fixtures which can be used with the 4284A?
Yes, all the test fixtures available for the 4284A can be used with the E4980A.

FAQ 2008-11-12

What is the size (dimensions) of E4980A-1CM rack mount kit?
The rack mount kit consists of a small bracket and a large attachment panel for installing the E4980A in a 19-inch standard rack as follows.

FAQ 2008-11-12

Can I use all fixtures and accessories that I'm using with the 4268A and the 4288A?
Yes, they can be used with E4981A.

FAQ 2008-10-20

How would I distinguish between old EEPROM (PN 1818-5719) and new one (PN 5183-4149) when transferring the EEPROMs to new CPU board?
It can be distinguished with the manufacturer part number on the top of the EEPROMs.

FAQ 2008-06-27

Is electrical length compensation required when using RF coaxial test fixture with the E4980A?
No, the electrical length compensation for RF coaxial test fixtures is not required.

FAQ 2008-06-11