这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 88

排序:
How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

Where can I find information on E4980A/AL error messages?
E4980A/AL error messages are described in Appendix B of the Users Guide.

FAQ 2017-06-28

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

微软终止支持 Windows XP,对我的 E4982A 有何影响?
自 2014 年 4 月 8 日起,微软已终止对 Windows XP 操作系统的支持。本文将帮助您回答某些重要的问题。

FAQ 2014-07-15

E4982A 硬件、软件和固化软件升级
E4982A 硬件、软件和固化软件升级

FAQ 2014-05-01

What are the differences between the E4980A and 4284A?
Most of the E4980A functions are compatible with the 4284A's. Since some enhancements and updates of functionality are incorporated in the E4980A, there are primary differences summarized in the table.

FAQ 2014-04-07

E4980A 和 42841A 之间的电缆的部件编号(P/N)是什么?
最新的电缆部件编号为 E4980-61640。

FAQ 2014-02-06

在 Keysight E4980A 中,什么是“直流电源选件 001(±10 VDC 最大值)”及其用法?
E4980A 选件 001 的增强性能概述——“增强功率和直流偏置选件”

FAQ 2012-12-02

Should I update I/O library version? (Automatic Update)
Keysight I/O Library is preinstalled in the E4982A.

FAQ 2012-10-25

PDF PDF
How should I set measurement points in BIN sorting of 4287A?
Setting of measurement points in BIN sorting of 4287A is independent of the selection of measurement points in the measurement display (single point measurement or list measurement).

FAQ 2012-08-01

How should I set measurement points in BIN sorting of E4982A?
Setting of measurement points in BIN sorting of E4982A is independent of the selection of measurement points in the measurement display (single point measurement or list measurement).

FAQ 2012-08-01

4285A 选件升级

FAQ 2012-07-24

为便于用户了解适当的阻抗测量技术,是德提供了哪些资源?

FAQ 2012-07-17

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

当在USB 闪存中保存测量数据时,为什么 E4980A 上偶尔会显示“E-230 数据损坏或失效”的错误消息?
当未能正确执行保存数据的程序时,或者当 USB 闪存不兼容 E4980A 时,便会出现以上情况。

FAQ 2011-07-24

哪种 USB 存储器件适用于 E4980A 和 E4981A?
建议使用 4 GB USB 存储器(Keysight PN 1819-0637)。

FAQ 2011-07-11

How can I know the stray capacitance and residual inductance values from OPEN A/B and SHORT A/B measurement data displayed on the E4980A LCD?
The E4980A displays the open admittance and the short impedance obtained for Open/Short compensation as OPEN A, OPEN B, SHORT A and SHORT B values on the CORRECTION Setup page.

FAQ 2011-06-07

Can the 16338A be used with LCR meters such as the 4263B and the E4980A?
No, the 16338A Test Lead Set doesn’t have compatibility with LCR meters. The 16338A can be used with the 4338A/B only.

FAQ 2011-06-07

How can the E4980A or the 4263B measure internal impedance of batteries?
Insert DC blocking capacitors between the measurement terminals and a battery DUT. The 16065C can substitute for the DC blocking capacitors.

FAQ 2011-06-07

E4980A/ 4263B/ 4284A/ E4981A 无法对特殊的测试夹具进行开路/短路补偿时,该如何检查测试夹具中的异常情况?

FAQ 2011-06-06

当直流偏置电流超过一定限度时,为什么 42841A 会关闭,而且在 E4980A/ 4284A 上还会显示“E25: DC bias I source overload”或“E26: DC bias I sink overload”错误消息?
42841A 输出的直流偏置电流不能超出由被测件直流电阻和直流输出电压最大极限值决定的电流限度。

FAQ 2011-04-21

When measuring a capacitor via a Keysight LCR meter, what is the best circuit mode, Cs or Cp?
To measure L, C, or R, there are two equivalent circuit models.The LCR meter can select the mode by setting the FUNC (function) to Cp, Cs, Lp or Ls.

FAQ 2010-09-30

Can I read a list sweep measurement data by operating the soft-panel of the E4980A on Web Browser?
Yes, you can read a list sweep measurement data using Web-server control mode.

FAQ 2010-09-19

How can I connect a test fixture to the measurement terminals of the E4980A when the stopper at the rear of the fixture disturbs the connection?
Remove the stopper from the test fixture by removing a screw at the center of the plastic stopper. Otherwise, remove the front rubber guide from the E4980A.

FAQ 2010-07-02

使用 Keysight 16085B 4 终端对至 7mm (APC-7) 适配器时,应使用夹具补偿标准件还是同轴校准标准件?

FAQ 2010-07-02

1 2 3 4 下一页