您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 36

排序:
SystemVue 影片庫
Keysight EEsof EDA 在 YouTube 上的 SystemVue 影片播放清單

基本展示 2019-01-09

How to Avoid Costly Mistakes in Designing Phased Array Systems
This video will show how to avoid 3 costly steps in designing a phased array. 1) Not predicting the failure of spurious emission masks (SEM) in simulation, which leads to higher development cost and missing time to market windows. 2) Not exploring thoroughly in one simulation, which leads to blind angles. 3) Relying primarily on spreadsheet calculations, which leads to longer design and development cycles.

使用說明影片 2018-02-01

IEEE 802.11ax: Overcoming Design and Test Challenges with 89600 VSA Software
The IEEE 802.11ax introduces various new technologies and features to meet its goal of higher efficiency, capacity and coverage for a better user experience, especially for dense deployment. These new technologies increase design complexity and create a number of new test challenges. This video covers key IEEE 802.11ax transmitter design and test challenges and how to overcome those challenges with Keysight’s 89600 VSA software.

基本展示 2017-10-02

IEEE 802.11ax: Physical Layer Overview
This video provides an overview of the IEEE 802.11ax WLAN standard highlighting the major physical layer technologies and features that are different from legacy WLAN standards.

基本展示 2017-10-02

IMS 2017: Top 5 Must-See 5G Products
Sponsored by Qorvo, Wireless Design and Development (WDD) counts down the best 5G products out of this year's International Microwave Symposium.

基本展示 2017-06-19

How to Design Phased Array Systems
This video presents the most important considerations for phased array system design, especially popular for proposed 5G architectures.

使用說明影片 2017-03-08

Keysight 5G Trial System Design and Validation Solution Demo
This video demonstrates Verizon’s early 5G trial system modeling connected to the latest 3GPP TR 38.900 mmWave channel model. These specifications facilitate early 5G trial system deployments and provide the wireless industry with the ability to test and validate key 5G technical components.

基本展示 2016-12-19

Transform 5G Concepts into “This Changes Everything” Reality
Evolve existing technologies. Invent new ones. Go from 5G waveform concept to “this changes everything" reality – while saving time, money and silicon. It starts with Keysight’s testbed for 5G waveform generation and analysis.

基本展示 2016-10-19

Unlocking Millimeter Wave Insights
It is easy to underestimate the challenges at millimeter-wave frequencies, and this amplifies the importance of integrated tools for design, simulation, measurement, and analysis. Learn more about how Keysight is taking the mystique out of millimeter waves and unlocking new insights.

基本展示 2016-09-30

Introducing SystemVue 2016
See a live demo of SystemVue 2016. The new capabilities enable researchers and system architects working on platforms using beamforming algorithms for 5G, satellite, NewSpace, radar and EW applications, to reduce interference and power consumption, while increasing physical range.

基本展示 2016-06-27

IMS-MTT 2016 from Keysight EEsof EDA
Highlights from Keysight EEsof EDA on the show floor at IMS-MTT 2016 in San Francisco, CA on May 22-26, 2016.

基本展示 2016-06-05

IMS 2015 Demos from Keysight EEsof EDA
YouTube video playlist containing International Microwave Symposium (IMS) 2015 demo videos from Keysight EEsof EDA MicroApps.

基本展示 2015-06-19

Microwave Journal - Keysight 5G Design and Verification
Microwave Journal video: 5G Applications Development Engineer Greg Jue demonstrates one of Keysight's latest innovations.

基本展示 2015-06-02

Microwave Journal - Keysight Interview with Todd Cutler
Microwave Journal Editor Pat Hindle interviews Todd Cutler, General Manager of Keysight EEsof EDA.

基本展示 2015-05-31

How to Understand 5G: Waveforms
This video will provide you with good guidance for understanding what kinds of new waveforms are being researched for the next generation standard. The example with end-to-end link level simulation will demonstrate waveform quality issues of a multi-carrier system and the nonlinearity from the RF chain.

使用說明影片 2015-05-01

Using SystemVue to generate IBIS AMI models
Use SystemVue to design your next gigabit SerDes link with great physical layer insights, and then quickly generate IBIS AMI models to act as a "transportable datasheet" for your design.

基本展示 2015-04-23

Discovering SystemVue - MATLAB Script Modeling
Keysight SystemVue now includes MATLAB Script, an equation and modeling engine from MathWorks. This product tutorial shows communications system designers how to create and debug MATLAB models from inside the SystemVue user interface.

基本展示 2015-04-15

5G 通道探量
這個影片討論了是德科技的 5G 毫米波 MIMO 通道探量解決方案。5G 的目標是實現隨時隨地的通訊,並將資料速率大幅提升到 gigabyte 等級。為此,我們需使用新技術,例如 massive MIMO 和 5G 毫米波寬頻解決方案。5G 的目標是實現隨時隨地的通訊,並將資料速率大幅提升到 gigabyte 等級。為此,我們需使用新技術,例如 massive MIMO 和 5G 毫米波寬頻解決方案。

基本展示 2015-03-19

Keysight 5G signal generation and analysis demonstration at Mobile World Congress
Keysight demonstrates candidate 5G FBMC waveform co-existence with 4G LTE, and up to 2GHz wideband FBMC signal generation and analysis using SystemVue W1906 5G library, N7608B Signal Studio for custom modulation, and 89600 VSA software applications with Keysight wideband test equipment.

基本展示 2015-03-09

Keysight 5G Millimeter-Wave Channel Sounding demonstration at Mobile World Congress
Keysight demonstrates a multi-channel Channel Sounding system at milimeter-wave frequencies, to enable 5G research and system validation

基本展示 2015-03-09

Keysight EEsof EDA Electronic System Level Design Flow with SystemVue
In this video we show the Electronic System Level, or ESL, design flow from Keysight based on SystemVue -- the fastest way to design and validate challenging physical layer communications systems, where baseband and RF must work together.

基本展示 2014-12-12

Realistic Ultra-Wideband Radar Signal Generation Using Keysight SystemVue
To lower test costs SystemVue can be used with Keysight test equipment to model realistic environment and jamming scenarios, which often involve costly outdoor ranges, chambers, and real-time hardware simulators. Watch the YouTube video to see how.

基本展示 2014-10-24

Design Challenges in DDR4 - The Keysight DDR Bus Simulator
This video is about design challenges in DDR4 and in particular the DDR Bus Simulator, which is a new Keysight EEsof EDA simulation tool for DDR4 and beyond.

基本展示 2014-10-16

Creating and Analyzing Multi Emitter Environment Test Signals with COTS Equipment
This presentation shows how wide‐bandwidth, multi‐channel digitizers can be used to capture and analyze signals.

基本展示 2014-08-14

Breaking the RF Carrier Barrier: 0-200 in Under a Second
Simulating nonlinear responses to hundreds of RF carriers is now practical with an innovative simulation technique.

基本展示 2014-08-01

1 2 下一頁