这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按内容类型

按产品类别

1-25 / 42

排序:
SENT Mask Files and Application Note
SENT mask files and an application note that describes how to use them with Keysight InfiniiVision oscilloscopes.

编程实例 2018-08-23

ZIP ZIP 429 KB
MATLAB IQtools
Example MATLAB application to generate multi-tone, pulsed radar, digital modulation and high-speed serial data signals. Works in conjunction with Keysight high-speed AWGs and Vector Signal Generators.

编程实例 2018-01-30

ZIP ZIP 3.29 MB
I/O 程序库示例程序
帮助您开始仪器编程的示例。

编程实例 2016-10-19

Sample Project Files for Automated NFC Test Software
Sample project files for the Automated NFC Test Software. To view: (1) extract files on the controller PC, (2) run the NFC Test App, (3) open the extracted .proj file.

编程实例 2016-07-25

ZIP ZIP
[实施方法] USB C 型电缆-连接器组件一致性测试

编程实例 2015-11-24

[实施方法] PCI Express 3.0 Tx/Rx 阻抗和回波损耗测试
[实施方法] PCI Express 3.0 Tx/Rx 阻抗和回波损耗测试

编程实例 2015-07-15

[实施方法] 以太网电缆测试

编程实例 2015-04-07

[实施方法] DisplayPort 1.3 电缆-连接器组件一致性测试
[实施方法] DisplayPort 1.3 电缆-连接器组件一致性测试

编程实例 2015-02-27

实施方法] USB 3.1 电缆-连接器组件一致性测试
实施方法] USB 3.1 电缆-连接器组件一致性测试

编程实例 2015-02-06

[实施方法]以太网发射机/接收机回波损耗测试

编程实例 2014-11-06

HDMI 源端/接收端阻抗测试

编程实例 2014-11-06

[Method of Implementation] MIPI D-PHY TxRx Interface S-parameter and Impedance Test

编程实例 2014-10-10

[实施法] BroadR-Reach 链路分段一致性测试

编程实例 2014-08-28

[Method of Implementation] USB 2.0 Cable-Connector Assembly Compliance Test

编程实例 2014-06-26

[Method of Implementation] SATA RXTX Impedance Compliance Test

编程实例 2014-04-28

[Method of Implementation] SATA SI Compliance Test

编程实例 2014-04-28

[Method of Implementation] MIPI M-PHY TxRx Interface S-parameter and Impedance Test

编程实例 2014-04-08

E5063A Sample Programs in Help
This is sample program files which are shown in the E5063A Help. See the E5063A Help for more detail.

编程实例 2014-02-01

Keysight VEE Pro Code Samples
These code samples demonstrate aspects of Keysight VEE Pro programming.

编程实例 2013-11-17

[实现方法] HDMI 电缆组件一致性测试
[实现方法] HDMI 电缆组件一致性测试

编程实例 2013-11-03

Command Expert 1.2 Examples Download
This archive contains instrument programming examples for Command Expert 1.2. Each example includes a programming sample written in Microsoft Excel, LabVIEW, MATLAB Instrument Control Toolbox, MATLAB Run Sequence, Keysight VEE, Visual Studio (C#/VB) SCPI.NET, Visual Studio (C#/VB) Run Sequence, and Visual C++ VISA.

编程实例 2013-05-20

ZIP ZIP 2.05 MB
[实施方法] DisplayPort 1.2b 电缆-连接器组件一致性测试
[实施方法] DisplayPort 1.2b 电缆-连接器组件一致性测试

编程实例 2013-04-18

[实施法] MHL 电缆至连接器组件一致性测试

编程实例 2013-03-28

[Method of Implementation] PCI Express 3.0 PCB Differential Trace Impedance Test

编程实例 2013-03-25

[Method of Implementation] USB 3.0 Cable-Connector Assembly Compliance Test

编程实例 2013-01-16

1 2 下一页