Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

1-25 sur 190

Tri:
The Case for Integrated Design Software
Design World article presenting the case for integrated design software by Lee Teschler.

Article 2019-10-22

X-Apps Marks the Spot - Essential Signal Analyzer Measurement Apps for Saving Test Time
Learn how measurement applications increase both the capability and functionality of signal analyzers, while reducing your time to measurement insights.

eBook 2019-10-08

PDF PDF
X-Apps Marks the Spot - Essential Signal Analyzer Measurement Apps for Saving Test Time - eBook
Learn how measurement applications increase both the capability and functionality of signal analyzers, while reducing your time to measurement insights.

eBook 2019-10-08

PDF PDF 4.24 MB
SECO Reduces DDR4 Board Failures to Zero and Design Optimization Time by 35%
As the speed of DDR technology increases, signal integrity becomes more challenging to maintain. To ensure reliable and accurate designs, they now require new tools and processes.

Étude de cas 2019-10-01

PDF PDF 2.10 MB
Design Team Increases Efficiency of High-Speed Digital Boards by 100%
Inspur Power Commercial Systems (IPS) found that Keysight’s PathWave Advanced Design System (ADS) contained all the tools and processes it needed to design stable, reliable high-speed digital PCBs.

Étude de cas 2019-09-24

PDF PDF 2.39 MB
Executive Interview: Todd Cutler, Keysight
Signal Integrity Journal caught up with Todd Cutler, Keysight’s VP and General Manager for Design & Test Software about product development, innovation, and the latest developments in SI/PI design.

Article 2019-09-19

Three Key Trends in Data Center Interconnects reach 400G Speeds and Beyond
Traditionally, coherent optical technology has been too expensive to use in data center interconnects, which are typically less than 80 km apart. New photonic integrated circuits and standards, such as 400ZR and IEEE 802.3ct, will enable physically separated data centers to cost effectively increase speeds to 400 Gb/s. These standards will ensure efficiency when sharing resources, balancing workloads, and scaling capacity.

eBook 2019-09-10

PDF PDF 3.11 MB
4 Real-World Applications for Electromagnetic Simulation
With the complexity of IC components increasing, EM circuit simulation is now critical for accurate and efficient design. With EM simulation, designers can account for EM effects on their circuit to avoid costly problems before they happen.

eBook 2019-09-09

PDF PDF 11.90 MB
IIT Kanpur Develops ASM-HEMT Model for GaN Transistors Using Parametric and Device Characterization
The India Institute of Technology Kanpur creates an accurate and simple compact SPICE model and introduces an industry-grade model for power electronics and RF applications.

Étude de cas 2019-07-10

PDF PDF 1.90 MB
Transforming Engineering Education with Cutting-Edge Keysight Labs
Keysight is committed to continue with innovation that will enable researchers, educators, and students.

Étude de cas 2019-06-25

PDF PDF 2.03 MB
Automaker Gets a 360 View of Radar Design and Test Validation with 50% Less Manpower - Case Study
A car maker saved 50% manpower by automating their tracking and fine-tuning systems for autonomous driving radio frequency (RF) tests with the Keysight PathWave laboratory management software.

Étude de cas 2019-06-19

PDF PDF 2.22 MB
Global EMS Manufacturer Reduces Time to Market Using PathWave Manufacturing Analytics - Case Study
The real time automated result analysis and anomaly detection in Keysight’s PathWave Manufacturing Analytics reduce engineering time and effort significantly, empowering the EMS company to release the product into the market sooner.

Étude de cas 2019-06-04

PDF PDF 2.09 MB
A Modern Approach to Satcom Design
Microwaves & RF article on satellite communication design written by Keysight Technologies' Wilfredo Rivas-Torres.

Article 2019-06-03

5G RF Design Startup Delivers Cutting-Edge GaN/GaAs Devices on Day One
To achieve success in the growing wireless industry, a company must deliver cutting-edge devices at competitive speeds. Doing so requires powerful design and simulation tools that can accurately measure the high frequencies that 5G demands.

Étude de cas 2019-05-10

PDF PDF 1.97 MB
Keysight EEsof EDA Newsletter - Product and Application News
Keep tabs on the latest product and application news and review the archives of the Keysight EEsof EDA Newsletter.

Bulletin d'information 2019-04-09

Probe Heatmap Visualization Tool Helps EMS Company Pinpoint a Costly Issue - Case Study
This case study demonstrate the success of PathWave Manufacturing Analytics helpung EMS company pinpoint and resolve a costly low first pass yield issue.

Étude de cas 2019-03-20

PDF PDF 1.97 MB
University Uses ADS to Create an Impedance Matching Method for Wireless Battery Charging
Learn how NCKU created an impedance matching method for wireless battery charging using Keysight ADS.

Étude de cas 2019-03-14

PDF PDF 2.27 MB
Ericsson and Freiburg U. Design High-Q Power Harvesting Circuit Using ADS
ADS HB was used to explore the design space around the innovative impedance transformation using a high Q quartz crystal resonator to transform the low voltage from the low impedance antenna.

Étude de cas 2019-03-14

PDF PDF 2.37 MB
Putting the Future in Motion with Automotive Ethernet
Continental adopts Keysight's automotive Ethernet test solution for 100BASE-T1, 1000BASE-T1, DDR memory, and USB connectivity compliance testing.

Étude de cas 2018-11-16

PDF PDF 3.30 MB
Different Strategies for Preparing Students to Tackle the RF Engineering Challenges of Tomorrow
Panel universities discuss the positive impact of leveraging Keysight’s RF and Microwave Education Programs to develop next generation RF industry-ready engineers.

Article 2018-09-04

PDF PDF 2.40 MB
Using Arduino in Engineering Education: Motivating Students to Grow from a Hobbyist to Professional
Keysight Technologies in collaboration with top US engineering schools have developed Arduino-based projects as motivators for advanced electronic engineering education in industrial setting.

Article 2018-08-27

PDF PDF 4.37 MB
Extending the Operating Life of IoT Devices with a Wireless Energy-Harvesting - Case Study
Geneva-based STMicroelectronics and French university Ecole Supérieure d’Electronique de l’Ouest (ESEO) collaborated on the development of “energy harvesting” circuits capable of transforming RF energy into DC power. STMicroelectronics and ESEO chose Keysight Advanced Design System (ADS) and its co-simulation capabilities to accurately design and simulate the rectifying circuit for the energy harvesting solution. The design team successfully created an energy-harvesting system that transformed ambient 2.45-GHz wireless signals into DC power.

Étude de cas 2018-08-20

PDF PDF 1.41 MB
Automotive & Energy Solutions - eBook
Automotive electronics is the underlying platform for all operations and diagnostics, convenience and comfort, safety and security, and main support for the three areas of innovation: e-mobility, autonomous driving, connected car.

eBook 2018-06-19

PDF PDF 4.31 MB
2017 Global Electronic T & M Software Competitive Strategy Innovation and Leadership Award
Frost and Sullivan awards Keysight Technologies the 2017 Global Electronic Test & Measurement Software Competitive Strategy Innovation and Leadership Award.

Article 2018-02-01

PDF PDF 2.89 MB
Creating an Impedance Matching Method for Wireless Battery Charging
NCKU researchers use ADS to develop a simple, yet effective DC-driving impedance matching method for rectifier-antennas and wirelessly charging implantable Li-ion rechargeable batteries.

Article 2018-01-01

1 2 3 4 5 6 7 8 Page suivante