Техническая поддержка
Электронные измерения
Уточнить список
По Отрасли/Технологии
По типу содержания
- Библиотека
- Руководство по применению
По типу оборудования
1-25 из 172
10 Hints for Making Successful Noise Figure Measurements - Application Note
This document will help minimize the uncertainties in your noise figure measurements. Key topics include minimizing extraneous signals, mismatch uncertainties, nonlinearities, and path losses.
Руководство по применению 2019-09-25 |
![]() |
P-Series Measurement Uncertainty Calculator
Measurement Uncertainty Calculator for the N1911A and N1912A Power Meters and the N1921A and N1922A Power Sensors.
Руководство по применению 2019-09-20 |
![]() |
Noise Figure Measurement Accuracy - The Y-Factor Method - Application Note
Specific to instruments that use the Y-factor method for noise figure measurements, this app note discusses measurement basics, avoidable errors, loss and temperature corrections, and uncertainties.
Руководство по применению 2019-03-19 |
![]() |
Making Conducted and Radiated Emissions Measurements - Application Note
This application note provides an overview of radiated and conducted emissions measurements as well as a methodology for EMI precompliance testing.
Руководство по применению 2019-03-08 |
|
Making Better Models with User Data
This paper details the process of combining MATLAB and the RF System analysis to improve the accuracy of simulations via personalized models.
Руководство по применению 2019-03-05 |
![]() |
EMI Compliance Test vs. EMI Pre-Compliance Test - Application Brief
This paper gives you an understanding on the advantage of running an in-house EMI pre-compliance test with a spectrum analyzer, guide you through the process of making a good estimation of your new product's EMI performance, and diagnose unwanted emissions.
Руководство по применению 2018-08-07 |
|
Testing and Troubleshooting Digital RF Communications Receiver Designs (AN 1314)
This Application Note covers the fundamental measurement principles involved in testing and troubleshooting digital communications
receivers, particularly those used in digital RF cellular systems. Measurement setups are provided for receiver performance tests and
troubleshooting tips are given.
Руководство по применению 2018-01-26 |
|
Signal Analysis Measurement Fundamentals, Optimize Noise Floor, Resolution Bandwidth, and More
Learn measurement fundamentals to optimize your signal analysis for greater insights
Руководство по применению 2017-12-13 |
|
Using Advanced Design System to Design an MMIC Amplifier
This AN illustrates the design of a MMIC amplifier, problems faced in designing, simulating, and producing a physical layout of an MMIC circuit, validation steps needed to verify that the physical layout.
Руководство по применению 2017-12-05 |
|
Preselector Tuning for Amplitude Accuracy in Microwave Spectrum Analysis
This 8 page application note introduces the technique for broadband modulated signals employed in the new MXA signal analyzer.
Руководство по применению 2017-12-05 |
![]() |
Optimizing RF and Microwave Spectrum Analyzer Dynamic Range - Application Note
This application note defines the elements of spectrum analyzer measurement speed and shows how to choose solution bandwidth and data output format for fast measurements.
Руководство по применению 2017-12-01 |
![]() |
Simulation and Verification of Pulse Doppler Radar Systems - Application Note
Keysight SystemVue illustrates key algorithms in modern Pulsed Doppler radar system design, and also connects to Keysight sources and signal analyzers to verify hardware performance.
Руководство по применению 2017-12-01 |
![]() |
One Size Does NOT Fit All - Application Note
This application note discusses the topic of “One Size Does NOT Fit All” and how test system configurations benefit from a choice of hardware form factors and software products.
Руководство по применению 2017-12-01 |
|
Average Power Sensor Measurement Uncertainty Calculator - Application Note
Measurement Uncertainty Calculator for the Average Power Sensors (N8481A, N8482A, N8485A, N8481A-CFT, N8482A-CFT, N8485A-CFT, 8481D, 8485D, 8487D, R8486D, Q8486D, E4412A, E4413A, E9300A, E9301A, E9304A, E9300B, E9301B, E9300H, E9301H)
Руководство по применению 2017-09-08 |
![]() |
Network Analysis - De-embedding and Embedding S-Parameter Networks (1364-1)
At RF and microwave frequencies, it becomes difficult to directly measure devices with nonstandard connectors (for example, devices using surface-mount packaging).
Руководство по применению 2017-09-07 |
![]() |
Fundamentals of RF and Microwave Noise Figure Measurements - Application Note
This 32-page, black-and-white application note providesinformation on RF and Microwave noise figure measurementts. Topics include noise figure and temperature, noise characteristics of two-port networks, and the measurement of noise figure.
Руководство по применению 2017-09-06 |
|
Новые методы анализа импульсных сигналов радиолокационных систем и средств радиоэлектронной борьбы
Настоящие рекомендации по применению
охватывают вопросы использования передовых средств измерений и новейших разработок для различных видов анализа импульсных сигналов, а также методы отображения и анализа для разных типов сигналов и измерительных задач.
Руководство по применению 2017-04-21 |
|
Genesys S/Filter Software Synthesizes Custom RF, MW and Analog Filters for Realization
This white paper describes direct filter synthesis capabilities in Keysight Genesys S/Filter design software used to realize custom filter response.
Руководство по применению 2016-09-23 |
|
Educational Overview of RF Power Measurement and Applications - Application Note
RF power measurement is the basic for the study of RF & microwave theories. Understand how RF power meter and sensor works and its applications from the educational perspectives.
Руководство по применению 2016-08-22 |
![]() |
Bluetooth Audio Measurement with the U8903B Performance Audio Analyzer - Application Note
This article focuses on the Bluetooth audio measurement applications of the U8903B performance audio analyzer. Bluetooth audio is also part of the whole audio measurement and analysis ecosystem.
Руководство по применению 2016-01-28 |
![]() |
5 Reasons to Buy the X-Series Noise Figure Analyzer - Flyer
This 2-page flyer lists 5 reasons to buy the X-Series noise figure analyzers
Руководство по применению 2016-01-26 |
![]() |
Проведение измерений ЭМП на соответствие требованиям стандартов - Рекомендации по применению
Данные рекомендации по применению описывают процесс проведения и подходы к измерению ЭМП
Руководство по применению 2015-07-25 |
|
Optimizing RF and Microwave Spectrum Analyzer Dynamic Range -- Application Note
The dynamic range of a spectrum analyzer is traditionally defined as the ratio, in dB, of the largest to the smallest signals simultaneously present at the input of the spectrum analyzer that allows measurement of the smaller to a given degree of uncertainty. The signals of interest can either be...
Руководство по применению 2015-07-24 |
|
Programming with the N937xA PXIe Vector Network Analyzers - Application Note
This application note discusses the process of developing a C# application using an IVI driver as the programming remote driver for the M937xA PXIe vector network analyzer.
Руководство по применению 2015-07-07 |
![]() |
Noise Figure Uncertainty Calculator
The noise figure uncertainty calculator has been created to aid your design work, from components through to systems, helping you meet the continued demand for higher system performance.
Инструмент для анализа 2015-05-29 |
|