이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-12 / 12

정렬방식:
Keysight Technologies Enters into Manufacturing Test License (MTL) Agreement with Broadcom

보도자료 2014-09-21

E6640A EXM Wireless Test Set Ready for Volume Production of LTE-A, 802.11ac WLAN Devices
Agilent Technologies today announced the E6640A EXM wireless test set, which offers breakthrough manufacturing-test scalability in technology coverage, performance and capacity to test up to 32 cellular and wireless-connectivity devices in parallel.

보도자료 2014-02-13

Agilent Technologies Releases New Software for X-Series Signal Analyzers
Agilent Technologies extended its leadership in 802.11ac WLAN test solutions with its latest measurement application release for X-Series signal analyzers. The software release offers expanded WLAN support to include the emerging 802.11ac standard.

보도자료 2012-11-01

Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

보도자료 2012-06-05

Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

보도자료 2012-05-01

Agilent Technologies Named Oscilloscope Company of the Year
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

보도자료 2012-04-25

Agilent Technologies Introduces Signal Processing Libraries for 802.11ac WLAN and 60-GHz 802.11ad
Agilent Technologies Inc. (NYSE: A) today released SystemVue 2011.10, the latest update to the leading design environment for wireless physical-layer architects.

보도자료 2011-11-16

Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

보도자료 2011-11-15

Agilent Technologies' PXA Signal Analyzer Now Enables Wideband Measurement with up to 900
Agilent Technologies Inc. (NYSE:A) today announced that its high-performance PXA signal analyzer now supports up to 900 MHz of intermediate-frequency bandwidth, enabling it to act as a broadband down converter for analysis of wideband communications and radar signals in aerospace and defense applications.

보도자료 2011-09-20

Agilent Technologies Introduces Wideband DPD Modeling Platform for LTE-Advanced, 802.11ac
Agilent Technologies Inc. (NYSE: A) today announced the newest release of its W1716 Digital Pre-Distortion Builder (DPD) software, designed to enable the high levels of wireless performance necessary for emerging wideband standards such as LTE-Advanced and IEEE 802.11ac.

보도자료 2011-08-31

Agilent Extends Wireless Leadership with First-To-Market Support for 802.11ac Design and Analysis
Agilent Technologies announces that its 89600B vector signal analysis software is now able to test 802.11ac signals. This is the first dedicated 802.11ac signal analysis solution on the market.

보도자료 2011-03-17

Agilent Technologies' New Attenuation Control Units Aid in WiMAX™, WLAN Device Testing

보도자료 2008-06-11