Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 56

Sort:
Why is the KCE cannot be launched in M9537A WES7?
If you need to access Keysight Connection Expert using the embedded controller with WES7, make sure you run Windows Update to install KB4041083, which is for .NET framework 4.6.2 Security and Quality Rollup.

FAQ 2020-10-29

Why is the GPIB driver missing from Device Manager in M9537A WES7?
If you need to access GPIB devices using the embedded controller with WES7, install IOLS version 18.1.24715.0. Newer versions of IOLS is known to have missing GIPIB drivers issue.

FAQ 2020-10-26

How do I activate Windows on my embedded controller?
Windows activation happens when the operating system is connected to the internet, it will take around 1-2 minutes to activate Windows depending on network bandwidth.

FAQ 2020-08-06

How to upgrade your Embedded Controller to Windows 10
You can easily update your Embedded Controller to Windows 10 by swapping out the SSD with a new Windows 10 SSD.

FAQ 2020-04-09

Why did my HostID change?
If there is a hardware change, most likely it will change the HostID of the system as well.

FAQ 2020-04-09

Where do I download the mechanical drawings for the M9502A?
Files can be imported into your modeling application.

FAQ 2020-03-23

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2020-02-06

Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2020-02-06

Where do I download the mechanical drawings for the M9506A?
Files can be imported into your modeling application.

FAQ 2019-09-10

What cable do you recommend for the M9203A I/O and Sync connectors?
Keysight cable U5300A-102, one of which is included with every M9203A order. This is 1 meter long, with MMCX (male) to BNC (male) connectors.

FAQ 2019-08-16

What is the Embedded Controller Default Password? Answer: Keysight4u!
The default password is “Keysight4u!” for the Administrator account for Windows 10 Enterprise 2016 LTSB. We recommend that you change the password for improved security, because the default password is public knowledge.

FAQ 2017-11-14

Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

Is there a PDF version available of the user guide for the M9210A? There are issues with the .chm file that is available.
No, there is not a PDF version available for the M9210A user manual. To read the .chm file, it must be downloaded and copied on the local C drive before opening.

FAQ 2017-06-28

Where do I download the mechanical drawings for the M9537A?
Files can be imported into your modeling application.

FAQ 2016-11-16

How do I setup for DisplayPort Hot Swap capability?
The M9537A has 3 DisplayPorts that are activated on boot-up. If you move a cable from one DisplayPort to another, you must reboot to activate the new configuration.

FAQ 2016-11-16

How do I make the AXIe module show up when there is an empty slot between it and the controller?
If you leave an empty slot between the M9537A controller and an AXIe module, you might not be able to use the AXIe module and an error will show up in Windows Device Manager.

FAQ 2016-11-16

How do I fix: unable to change GPIB settings on an M9037A or M9537A Embedded Controller?
Make the following changes...

FAQ 2016-08-27

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

Where do I download the mechanical drawings for the M9505A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9514A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9521A?
Files can be imported into your modeling application.

FAQ 2016-01-08

All M9202A PXI Express 12-bit Wideband IF Digitizer IVI and MATLAB Instrument Drivers
Supported models: M9202A

FAQ 2014-08-12

L453xA: Is there any way to implement LXI class B synchronization over large areas?
The L453xA digitizer does not support LXI class B directly. However consider using...

FAQ 2014-04-07

What type of internal memory is installed into the L4532A/34A LXI Digitizers?
Please refer to the document linked to this page for a comprehensive listing of memory installed into the Keysight L4532A/34A LXI Digitizers.

FAQ 2014-04-07

How do I connect multiple PXIe and/or AXIe chassis together with a single controller?
PXIe and AXIe chassis can be interconnected in multiple configurations.

FAQ 2013-08-07

1 2 3 Next