Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

26-50 of 50

Sort:
How do I enter my own antenna correction factors on the ESA or EMC Series Analyzer?
Access the AMPLITUDE, More, Corrections menu.

FAQ 2008-11-21

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

Is it OK to connect both AC and DC power sources to my ESA Series Spectrum Analyzer simultaneously?
No, damage to the instrument or the 12Vdc source may occur!!

FAQ 2008-11-21

When should I press "Discharge DC Block Capacitor" softkey of the E5052B?
It is recommended to press this softkey when reconnecting the DUT at the baseband input port of the E5052B.

FAQ 2008-10-22

Why does the built-in speaker of my E7400A EMC and ESA Analyzer appear to cut out while demodulating signals?
This is due to the internal auto alignment routine...

FAQ 2008-10-09

Is there any way to reduce the intensity of the display on an ESA or EMC spectrum analyzer if it must be left on for long periods of time?
Not via the Front Pannel but can be done using a SCIPI command. See text...

FAQ 2008-10-09

Can I select different display color schemes on the E7400A Series EMC and the ESA-E Series Analyzers?
Yes. See content for details...

FAQ 2008-10-09

How many files can be saved to a floppy disk in the ESA or EMC spectrum analyzer?
Approximately 80 screen images and 100 trace files.

FAQ 2008-10-09

In the ESA-E Series, is the High Stability Frequency Reference (Option 1D5) powered while it is in Standby?
No... See content for details...

FAQ 2008-10-09

What is the purpose of the Power ON Selection DIP switch located on the rear of my E7400A EMC and the ESA Analyzer?
See content for details...

FAQ 2008-10-09

What are the default logins and passwords for the N9039A RF Preselector?
User name = instrument, Password = measure4u. See FAQ content for more details...

FAQ 2008-07-01

How do I save the instrument state on my N9039A RF Preselector?
The preselector state is saved along with the PSA state when it is saved in EMC Analyzer mode...

FAQ 2008-07-01

I press Mode Preset on my N9039A RF Preselector but I still don't see any softkey labels. What's wrong?
Try pressing the front panel "Full Screen" key...

FAQ 2008-07-01

I press front panel keys on my N9039A RF Preselector but I get no response on the display. What's wrong?
Either the preselector application is not the active window or you are under remote control...

FAQ 2008-07-01

Why is the sweeptime so long on my EMC analyzer when I select the Quasi-Peak Detector?
Because of the CISPR 16-1 specified time constants for one.......

FAQ 2008-06-27

Is the VGA output of the ESA and EMC Series Analyzer monochrome or color?
On both product families, the output is color.

FAQ 2007-12-20

How can I use the Rear Panel DC Input Connector on my ESA/EMC Series Spectrum Analyzer?
The ESA/EMC will run on DC power via the Option A5D DC Input cables or the E1779A Battery pack.

FAQ 2007-12-20

What do "R", "L", "T", and "S" refer to in the upper-righthand portion of the analyzer's display?
See content for details...

FAQ 2007-12-20

What is the difference between video and power averaging types on the ESA Series Spectrum Analyzers?
Video should be used when in a LINEAR scale, Power should be used when in a LOG scale.

FAQ 2007-12-20

Is it possible to save a full-sized screen capture, without the softkeys?
Yes... See content for details...

FAQ 2007-12-20

How do I troubleshoot E5500 GPIB connectivity?
Here is the procedure to follow if there is a problem with instrument connections via GPIB with the E5500 software.

FAQ 2007-10-18

Is there a master listing of compatible printers for various network analyzers and impedance analyzers?

FAQ 2007-07-10

How do I change the signal path settings from the front panel on my N9039A RF Preselector?
From the PSA controlling it.

FAQ 2007-05-31

How do I tune the frequency of my N9039A RF Preselector?
From the PSA controlling it...

FAQ 2007-05-31

8903B, Source Impedance Switch

FAQ 2002-06-27

Previous 1 2