这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-25 / 47

排序:
Do I need to perform a periodic front panel instrument alignment on my N9039A RF Preselector?
No, but there is a system alignment that needs to be periodically run. See FAQ content for details...

FAQ 2012-12-11

What is the measurement uncertainty for the 8902A Option 50?
The only uncertainty in the 8902A Option 050 test system should be the accuracy of the attenuation source.

FAQ 2012-05-30

What Options would my PSA Series Spectrum Analyzer require to operate in an N5530S / N5531S Measuring Receiver system?
It is highly recommended that your PSA have with Option 1DS (100 kHz to 3 GHz Preamplifier) or Option 110 (10 MHz to 26.5 GHz / 50 GHz preamplifier) for improved dynamic range.

FAQ 2012-03-15

When should I "Restart" the N5530S Measuring Receiver software and how?
The easiest way to "Restart" measurement is to press "F5" button on your PC keyboard.

FAQ 2012-02-28

How do I include Mismatch Uncertainty into the N5530S Measuring Receiver Absolute Amplitude accuracy?
See content for details...

FAQ 2012-02-27

Why does the N5530S Measuring Receiver require Option 123 (Preselector Bypass) above 3 GHz?
Preselector drift introduces errors to the amplitude measurements.

FAQ 2012-02-27

Does the N5530S Measuring Receiver require a system calibration to meet specifications?
The N5530S does not require a system calibration. Its specifications are based upon the power meter and PSA performance.

FAQ 2012-02-26

Why is the marker Count Accuracy on the on the ESA Series Spectrum Analyzer only specified when using resolution bandwidths >1KHz?
If more that one signal is present in the 1kHz span, the marker count will be incorrect.

FAQ 2010-09-08

How can I make phase noise measurements on my 89400 series vector signal analyzer (VSA)?
The attached procedure takes you step-by-step through a phase noise measurement on the 89441A using two methods: direct spectrum and PM demodulation.

FAQ 2010-05-16

N5532A 传感器模块的频率范围是多少?
100 kHz 至 4.2 GHz,10 MHz 至 18 GHz,30 MHz 至 26.5 GHz 和 30 MHz 至 50 GHz。

FAQ 2010-04-13

What are the major differences between the 859xEM EMC Analyzers and the 859xE Spectrum Analyzer families?
The 859xEM EME Analyzer family comes standard with pre-loaded options specifically for EMC precompliance measurements.

FAQ 2004-06-22

Do the 8590EM Series EMC Analyzers have the 1MHz 6dB EMI bandwidth?
Yes, they do....

FAQ 2004-06-22

Is there a replacement for the 85878A EMI Report Generator Software?
Not exactly. See text for further information on this topic....

FAQ 2004-03-30

8903A, 8903B, 8903E比较
Keysight 是Keysight 8903A的替代产品。

FAQ 2003-11-24

Keysight 8542E/8546A: What External Monitor Works With This Instrument?

FAQ 2002-06-27

8901B LO Feedthrough out the RF Input Port

FAQ 2002-06-27

8903B Output Impedance

FAQ 2002-06-27

8901A, 8901B, 8902A Extending the Frequency Range
In normal operation the 8901, 8902 uses only the fundamental component of the internal local oscillator (LO).

FAQ 2002-06-27

8901A, 8901B Discrepancy Between FM Deviation Measurements
It was found that the FM Deviation measurement is slower in the 8901B than in the 8901A. The reason is that the 8901B and 8902A share firmware that is a little slower when reading the voltmeter and converting to FM dev.

FAQ 2002-06-27

8903, Quasi-Peak Detection, Signal-to-Noise Measurements

FAQ 2002-06-27

8901, 8902 Modulation Output Noise

FAQ 2002-06-27

8903B, Output Power, 8904A Option 006

FAQ 2002-06-27

8903B, AC Level Measurement, Speed Improvement

FAQ 2002-06-27

Keysight 8902A, Error 33, Error 34 TRFL, Tuned RF Level Mode

FAQ 2002-06-27

8903B, Residual Distortion and Noise

FAQ 2002-06-27

1 2 下一页