이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 311

정렬방식:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2020-05-22

신호 및 스펙트럼 분석기 벤치탑/모듈러/핸드형 펌웨어 업데이트 센터
벤치탑 및 핸드형 모델의 신호 및 스펙트럼 분석기용 펌웨어 또는 소프트웨어 최신 버전 액세스.

FAQ 2019-07-11

How do I upgrade my E7400A Series EMC Analyzer?
Find Information on Hardware Upgrades, Instrument Software, etc…

FAQ 2019-06-11

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2016-07-05

30-Day Free Trial for X-Series Measurement Applications for X-Series Modular Instruments
30-day trial license available for the X-Series measurement applications for X-Series modular signal analyzers.

FAQ 2016-06-09

E5053A 및 11970 믹서를 포함한 E5052B의 위상 노이즈 감도란 무엇입니까?
이 문서를 참조하십시오.

FAQ 2016-03-29

키사이트, 애질런트 및 휴렛팩커드의 단종된 테스트 장비에 대한 매뉴얼은 어디에서 확인할 수 있습니까?
대부분의 키사이트 제품의 PDF 매뉴얼은 제품 페이지에서 확인하실 수 있습니다. 다른 벤더들도 예전 매뉴얼을 제공합니다.

FAQ 2014-08-01

E5052B 하드웨어, 소프트웨어 및 펌웨어 업그레이드
E5052B 하드웨어, 소프트웨어 및 펌웨어 업그레이드

FAQ 2014-08-01

Microsoft Windows XP의 지원이 종료되면 현재 사용하는E5052B에는 어떤 영향을 미칩니까?
Microsoft는 2014년 4월 8일자로 Windows XP 운영 체제에 대한 지원을 중단합니다. 이 문서는 중요한 질문에 답변하는 데 유용할 것입니다.

FAQ 2014-08-01

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

What is the RF Test Blog?
RF engineers know that making good measurements is a challenge. The RF Test Blog was created as a resource for RF engineers to find ways to make better RF measurements.

FAQ 2013-12-17

How do I correctly enter and use the correction factors for a current probe such as the 11967A/B with an X-Series Signal Analyzer?
See FAQ content for information on this.

FAQ 2013-10-16

How do I correctly enter and use the correction factors for a current probe such as the 11967A/B with an E7400A Series EMC
See FAQ content for information on this.

FAQ 2013-04-24

I lost my E5500 Phase Noise System license key. How do I obtain a permanent replacement license key?
In order to obtain a permanent replacement phase noise system license key the phase detector test set (70420A or N5500A) serial number is required.

FAQ 2012-12-20

How often does the system user alignment for the PSA EMI Measurement Receiver need to be run?
30 days or 3° C temperature change. See contents for details...

FAQ 2012-12-11

Do I need to perform a periodic front panel instrument alignment on my N9039A RF Preselector?
No, but there is a system alignment that needs to be periodically run. See FAQ content for details...

FAQ 2012-12-11

PXA의 External Mixing Mode에서 Phase Noise 측정이 가능합니까?
예, 가능합니다.

FAQ 2012-10-25

For my PSA Series Spectrum Analyzer, what is recommended to do if my instrument is having trouble saving files or the instrument firmware is unexpe...
This issue may be caused by a corrupt firmware file or may be caused by a defect in firmware. Please first try upgrading the instrument’s firmware to the latest version posted on the Keysight web. This issue may also be caused by a hardware probl...

FAQ 2012-05-30

What is the measurement uncertainty for the 8902A Option 50?
The only uncertainty in the 8902A Option 050 test system should be the accuracy of the attenuation source.

FAQ 2012-05-30

Can I get a temporary license key for my PSA Series, ESA Series, or EMC Series Analyzer?
No. At this time, we do not have temporary licenses. License keys for these instruments are generated based on the serial number, model number, and Host ID.

FAQ 2012-05-28

How do I transfer the screen image on my PSA, ESA, or EMC analyzer to a PC using Keysight VEE?
See content for complete details and an example program...

FAQ 2012-03-16

How long does the system user alignment of my PSA EMI Measurement Receiver take to run?
A full system alignment takes approx. 30 minutes. See FAQ content for further details...

FAQ 2012-03-16

What should I do if the system user alignment of my PSA EMI Measurement Receiver fails?
This could be caused by a few different reasons. See contents for details...

FAQ 2012-03-16

How do I transfer the current Signal List in my E7400A EMC Analyzer to my PC using remote commands?
First save the list to a file inside the instrument and then transfer the file.

FAQ 2012-03-16

1 2 3 4 5 6 7 8 9 10 ... 다음