Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 37

Sort:
Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

How often does the system user alignment for the PSA EMI Measurement Receiver need to be run?
30 days or 3° C temperature change. See contents for details...

FAQ 2012-12-11

Do I need to perform a periodic front panel instrument alignment on my N9039A RF Preselector?
No, but there is a system alignment that needs to be periodically run. See FAQ content for details...

FAQ 2012-12-11

Why does my PSA EMI Measurement Receiver tell me that I need to run the user alignment everyday?
There are a couple of reason why this could be hapening. See FAQ contents for details...

FAQ 2012-03-16

How do I erase/clear the user data in an ESA or EMC series spectrum analyzer for security reasons?
Follow this link for further information....

FAQ 2012-03-16

Why don't the Measure at Marker or Auto Measure peak detector values match the peak trace marker values on my EMC analyzer?
Your instrument firmware may need to be updated....

FAQ 2012-03-16

What does the system user alignment of my PSA EMI Measurement Receiver do?
See contents for details...

FAQ 2012-03-16

Why does my signal go off the top of the screen when I select either the Quasi-Peak or EMI Average detectors in my EMC or ESA analyzer?
Your instrument firmware may need to be updated to fix an auto ranging problem....

FAQ 2012-03-16

What should I do if the system user alignment of my PSA EMI Measurement Receiver fails?
This could be caused by a few different reasons. See contents for details...

FAQ 2012-03-16

How long does the system user alignment of my PSA EMI Measurement Receiver take to run?
A full system alignment takes approx. 30 minutes. See FAQ content for further details...

FAQ 2012-03-16

Why do spurious signals appear in my spectrum analyzer span when I apply a clean signal to the RF input?
Overdriving the input mixer of the analyzer may cause the spurs.

FAQ 2012-02-26

How do I save my trace data in a comma-separated variable (.csv) file format on an ESA, PSA or EMC spectrum analyzer?
On the front panel of the analyzer, press [File]{Save} and select either the A: (floppy) or C: (internal) drive...

FAQ 2012-02-24

What are the differences between an E7400A Series EMC Analyzer and an ESA Series Spectrum Analyzer with Option AYQ - EMI Detectors & FM Demod?
See table provided....

FAQ 2011-07-07

What signal sources are support for use as an alignment source for the PSA / N9039A RF Preselector based system?
8648B / N5181A / N5182A / N5183A/ N5161A / N5162A / E4438C / E8257D

FAQ 2010-09-08

Why is the marker Count Accuracy on the on the ESA Series Spectrum Analyzer only specified when using resolution bandwidths >1KHz?
If more that one signal is present in the 1kHz span, the marker count will be incorrect.

FAQ 2010-09-08

How do I enter my own antenna correction factors on the ESA or EMC Series Analyzer?
Access the AMPLITUDE, More, Corrections menu.

FAQ 2008-11-21

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

Is it OK to connect both AC and DC power sources to my ESA Series Spectrum Analyzer simultaneously?
No, damage to the instrument or the 12Vdc source may occur!!

FAQ 2008-11-21

In the ESA-E Series, is the High Stability Frequency Reference (Option 1D5) powered while it is in Standby?
No... See content for details...

FAQ 2008-10-09

How many files can be saved to a floppy disk in the ESA or EMC spectrum analyzer?
Approximately 80 screen images and 100 trace files.

FAQ 2008-10-09

Is there any way to reduce the intensity of the display on an ESA or EMC spectrum analyzer if it must be left on for long periods of time?
Not via the Front Pannel but can be done using a SCIPI command. See text...

FAQ 2008-10-09

What is the purpose of the Power ON Selection DIP switch located on the rear of my E7400A EMC and the ESA Analyzer?
See content for details...

FAQ 2008-10-09

Can I select different display color schemes on the E7400A Series EMC and the ESA-E Series Analyzers?
Yes. See content for details...

FAQ 2008-10-09

Why does the built-in speaker of my E7400A EMC and ESA Analyzer appear to cut out while demodulating signals?
This is due to the internal auto alignment routine...

FAQ 2008-10-09

1 2 Next