您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-6 / 6

排序:
當我將 Keysight N6700 系列 DC 電源供應器模組裝入主機並打開設備電源時,前面板上會出現錯誤訊息 207。這個錯誤訊息是什麼意思?我該如何讓此訊息不再出現?
錯誤訊息 207 表示「校驗檔案版本錯誤」,這表示在 Keysight N6700B 主機中使用了較新的韌體版本進行校驗。

FAQ 2012-07-30

How Do I Find My Host Information?
The Host ID is the model and/or serial number of the product, both of which can be found on the serial number label on the back of the instrument.

FAQ 2012-06-14

What is the part number for the output connector for the N67XX?
This information is found on pg 24 of the N6700B user guide.

FAQ 2011-07-08

What are the differences between the Keysight N6705A DC Power Analyzer and the N6705B DC Power Analyzer?
The N6705B mainframe has new labeling that identifies which knobs have secondary functions when you press them...

FAQ 2010-08-09

What does the LGA option on the N6751A and N6752A modules offer?
The LGA option is strongly recommended on the N6751A/52A modules. The LGA option stands for Large Gate Array.

FAQ 2009-12-20

如果打算在 Keysight N6705A 直流電源暨分析儀上使用直流電源模組,需要訂購 Keysight N6751A、N6752A 和 N6754A 高效能直流電源模組的選項 054 (高速測試擴充模組) 嗎?
在直流電源暨分析儀上使用直流電源模組時,並不需要選項 054。

FAQ 2007-11-04