Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 36

Sort:
Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

66xxA, E363xA and E364xA: Ca Keysight Power Supplies Sink Current?
Yes! Sinking, or down-programming, is the ability to pull current into the positive terminal of a power supply.

FAQ 2013-01-22

When I put a N6700 family DC Power Supply module into my mainframe, I get error 207 listed on the front panel when I turn the unit on. What does th...
Error 207 means “calibration file version error”. This means that the module was calibrated in a N6700B mainframe with a version of firmware that is newer than the version of firmware in the mainframe where it is generating the error.

FAQ 2012-07-30

How Do I Find My Host Information?
The Host ID is the model and/or serial number of the product, both of which can be found on the serial number label on the back of the instrument.

FAQ 2012-06-14

What is the part number for the output connector for the N67XX?
This information is found on pg 24 of the N6700B user guide.

FAQ 2011-07-08

66xxA and E36xxA: Determining Power Supply Constant Current Mode
The power supply cannot be "put" into the constant current mode.

FAQ 2010-08-27

What are the differences between the Keysight N6705A DC Power Analyzer and the N6705B DC Power Analyzer?
The N6705B mainframe has new labeling that identifies which knobs have secondary functions when you press them...

FAQ 2010-08-09

66000A: Setting Dwell Time
The List mode can contain up to 20 Voltage, Current or Dwell steps if controlled over the GPIB, or up to 8 steps if controlled from the optional keyboard...

FAQ 2010-05-26

661xC and 663xB: Power Supply Output Transition Time

FAQ 2010-05-16

What does the LGA option on the N6751A and N6752A modules offer?
The LGA option is strongly recommended on the N6751A/52A modules. The LGA option stands for Large Gate Array.

FAQ 2009-12-20

662xA: Replacing GPIB Printed Circuit Board Assembly

FAQ 2009-03-30

For N6700 series power supply, can the option 054 be upgraded after purchase?
Sorry, but the only solution is to order a new module with Option 054 High-Speed Test Extensions. Currently Keysight doesn't stock any hardware or software to add options to modules after the customer orders it.

FAQ 2008-10-21

66xxA, 68xxB, N330A and E36xxA: Determining the Correct Line Voltage Option to Order for a Power...
Some power products use lots of power, far beyond the range of typical electronic products with which we are familiar. This makes choosing the correct line voltage option more challenging.

FAQ 2008-09-22

66xxA and E36xxA: Programmable Current Sinking
In general, current sinking is a fixed value at some percentage of the full scale current output. However, there is an exception for one series of Keysight power supplies. On the 663xB series, the maximum negative current tracks the value programme...

FAQ 2008-09-22

66xxA: Calibration Certificates
Criteria have been established to determine which products get or do not get a calibration from the factory. A product with a product number does not automatically qualify for a calibration certificate.

FAQ 2008-09-22

66xxA, E362xA, E363xA, E364xA: DC Power Supplies Connecting in Series or in Parallel
The resultant voltage for series connections cannot exceed the maximum floating voltage allowed for any on the component power supplies. While this is typically +/-240 volts dc, there are some supplies as low as +/-25 volts dc, and others as high ...

FAQ 2008-09-22

66xxA and E36xxA: P-P Voltage Noise Versus RMS Noise
Both Vp-p and Vrms are measures for the unwanted AC components of a DC power supply output. Peak-to-peak noise is measured from the maximum positive point on the waveform to the most negative voltage point.

FAQ 2008-09-22

66xxA: Re-Calibration Date
There are no components used in Power Products which have a specific shelf life. Therefore, the calibration period of this instrument begins on the date that the product is first put into service by the customer. The recommended calibration interv...

FAQ 2008-09-22

Why doesn't my System Power Supply accept commands over the GPIB?
If you are getting either error 11 or error 113 when you try to send GPIB commands to your system supply, it may be that you are using the wrong command language.

FAQ 2008-07-29

Do I need to order option 054 (High Speed Test Extensions) for the N6751A, N6752A, and N6754A High Performance DC Power Modules, when I plan on usi...
Option 054 is not required when the DC Power Module will be used in a DC Power Analyzer.

FAQ 2007-11-04

How can I offset the voltage drop caused by long cable lengths from my dc power supply to the device under test (DUT)?
Normally, Keysight power supplies are delivered configured to deliver their full specs at the output terminals. In some application, where long lead lengths to the DUT are unavoidable, the regulation of the power supply at the DUT can be significan...

FAQ 2007-06-01

66xxA, E435xB, 605xB, N3300A and E36xxA: 'Floating' the Output of a Power Supply Above Ground
66xxA, E435xB, 605xB, N3300A and E36xxA: 'Floating' the Output of a Power Supply Above Ground

FAQ 2006-10-21

How do I clear non-volatile memory locations for security purposes?
For Keysight Model 66000A, each module has 5 states where data can be saved (0 to 4). State 'zero' is the wake-up state. To clear all states, save ZERO into each state.

FAQ 2006-10-21

60xxA, 66xxA and 663xx: Transient Current Overshoots above the Current Limit Setting for Power...
Transient Current Overshoots above the current limit setting for power

FAQ 2005-02-14

66xxA, 68xxB and N330xA: Power Products Memory

FAQ 2003-11-04

1 2 Next