这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-25 / 93

排序:
利用现代台式电源节省时间
是德科技的全新低成本直流台式电源拥有三路独立的输出,并且内置数据记录器。请看这些现代的台式电源能为您提供什么帮助。

FAQ 2017-06-20

How can I source a sinusoid waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-12-24

How can I source an exponential waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-12-24

What is the difference among data query commands such as ":FETCh?", ":MEASure?", ":READ?", :SENSe:DATA?"?
They have the function to query data similarly but there is some difference among them. Click the above link for details.

FAQ 2013-09-16

How can I source a pulsed signal on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-09-16

What is the difference among Trigger Types on Single View?
Click the above link for details.

FAQ 2013-09-16

What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?
It should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous. Once you send it with the parameter "ON", the parameter is set to "END VALUE".

FAQ 2013-09-16

我可以在哪里找到是德科技、安捷伦和惠普的已停产测试与测量设备手册?
是德科技的大部分产品页面都能提供 PDF 版本手册。另外,其他厂商也可能提供旧版手册。

FAQ 2013-05-29

The Keysight B2961A/B2962A shows the message "Interlock terminal is open" and don't accept to input voltage more than 42 V.
Click the above link for details.

FAQ 2013-03-11

How can I find the sensing type of the channels on the B2961A/B2962A?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2013-03-11

Can I upgrade from B2961A to B2962A?
No, you cannot upgrade from B2961A to B2962A.

FAQ 2013-03-11

How can I find the power-on program setting of the B2961A/B2962A?
You can find the power-on program setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

How can I update its firmware on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How can I find the power-on state setting of the B2961A/B2962A?
You can find the power-on state setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

Quick I/V Measurement Software cannot recognize the B2961A/B2962A.
The B2961A/B2962A is supported by Quick I/V Measurement Software in the revision 2.0 or later. Click the above link for details.

FAQ 2013-03-11

How can I set up Power-on State of the B2961A/B2962A?
It is possible to store the desired instrument condition as Power-on State. Click the above link for details.

FAQ 2013-03-11

How can I perform a self calibration on B2961AB2962A?
Click the above link for details.

FAQ 2013-03-11

How can I save or load the measurement setups on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How can I enable Over Voltage/Current Protection function on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How to configure the time constant of the output filter with the B2961A/B2962A?
The time constant of the output filter can be configured on the Output Filter dialog box. Click the above link for details.

FAQ 2013-03-11

How can I find the low terminal state of the channels on the B2961A/B2962A?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2013-03-11

What kind of interface can I use to control the B2961A/62A?
The GPIB, USB and LAN are available to control the B2961A/62A.

FAQ 2013-03-11

How can I configure Trigger Output Signals with the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

Where can I get LabVIEW Plug and Play Instrument Driver for B2961A/B2962A?
You can get LabVIEW Plug and Play Instrument Driver for B2961A/B2962A from NI.com.

FAQ 2013-03-11

Can B2961A/B2962A connect its output to the ground when the output is switched off?
Yes, the B2961A/B2962A can connect its output to the ground by specifying the output-off state to "ZERO" when the output is switched off.

FAQ 2013-03-11

1 2 3 4 下一页