Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-6 of 6

Sort:
Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12