Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

26-50 of 129

Sort:
Can the B2961A/B2962A step the source value immediately after the value is changed by its rotary knob?
Yes, it's possible by enabiling Immediate V/I Update function. Click the above link for details.

FAQ 2013-03-11

I can't source as low noise signal as expected from the B2961A/B2962A with the Low Noise Filter.
Click the above link for details.

FAQ 2013-03-11

I can't source as low noise signal as expected from the B2961A/B2962A with the Ultra Low Noise Filter.
Click the above link for details.

FAQ 2013-03-11

How to configure the time constant of the output filter with the B2961A/B2962A?
The time constant of the output filter can be configured on the Output Filter dialog box. Click the above link for details.

FAQ 2013-03-11

How can I find the power-on state setting of the B2961A/B2962A?
You can find the power-on state setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

How can I find the power-on program setting of the B2961A/B2962A?
You can find the power-on program setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

How can I configure Trigger Output Signals with the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

66xxA, E363xA and E364xA: Ca Keysight Power Supplies Sink Current?
Yes! Sinking, or down-programming, is the ability to pull current into the positive terminal of a power supply.

FAQ 2013-01-22

How do I find my Keysight B2961A/B2962A firmware revision?
You can find the firmware revision on the Revision dialog box.

FAQ 2012-12-30

Is it possible to append the data to the previous one in Graph View?
No.

FAQ 2012-12-30

How can I source a square waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2012-11-22

How can I source a trapezoid waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2012-11-22

How can I source a ramp waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2012-11-22

What is the interlock feature of the Keysight B2961A/B2962A?
Click the above link for details.

FAQ 2012-11-22

How can I source a triangle waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2012-11-22

Can I use N1294A-001/002 banana-triaxial adapter with B2961A/62A?
Yes, it is recommended that the banana-triaxial adapter should be used with B2961A/62A in the case of < 1nA sourcing.

FAQ 2012-11-11

Can ULNF and LNF be used with the B2901/02/11/12A?
No. Using these optional filters with the Keysight B2901/02/11/12A SMUs is not recommended.

FAQ 2012-11-01

When I put a N6700 family DC Power Supply module into my mainframe, I get error 207 listed on the front panel when I turn the unit on. What does th...
Error 207 means “calibration file version error”. This means that the module was calibrated in a N6700B mainframe with a version of firmware that is newer than the version of firmware in the mainframe where it is generating the error.

FAQ 2012-07-30

How Do I Find My Host Information?
The Host ID is the model and/or serial number of the product, both of which can be found on the serial number label on the back of the instrument.

FAQ 2012-06-14

Why did the current overshoot my current limit, and what is mode crossover?
The simplest description of mode crossover is the transition between one mode of operation to another, such as CV to CC...

FAQ 2011-08-16

What is the part number for the output connector for the N67XX?
This information is found on pg 24 of the N6700B user guide.

FAQ 2011-07-08

What is the best way to ensure simultaneous triggering of multiple units of modular products?
Using the cardcage, U2781A is the best way of ensuring simultaneous triggering of multiple units

FAQ 2010-12-20

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

What does the check mark at the rear panel label of the E3600 series bench power supply mean?
The check mark on the rear panel label shows the AC power rating for this unit which shipped from the factory.

FAQ 2010-09-20

Why some bench power supply comes with yellow label stating 100V ONLY or 115V ONLY?
The main purpose of the yellow label (as shown below) is to caution customer ...

FAQ 2010-09-20

Previous 1 2 3 4 5 6 Next