이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 41

정렬방식:
What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

M8000 시리즈를 위한 30일 무료 체험판 라이선스
M8000 제품군 내의 모든 체험판 라이선스에 대한 개요 및 링크

FAQ 2017-01-31

What do the output channels look like?
81110A/ 12A, 81130A/ 31A/ 32A의 출력 채널 회로도를 참고하십시오.

FAQ 2015-07-22

How much programming compatibility does exist between 81101A, 81104A, 81110A and 81150A, 81160A?
The implemented 81150A, 81160A SCPI command set is based on Keysight’s 81101A, 81104A, 81110A Pulse Pattern Generator product family. Therefore, most of the commands available for that instrument family are also available in the 81150A, 81160A models.

FAQ 2013-03-21

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

What is the best configuration for wideband I/Q modulation?
An E8267D Option 016 or an N8212A Option 016 signal generator with an M8190A arbitrary waveform generator

FAQ 2012-12-28

Typical Propagation Delay for the 81110A/11A
Refer to the image showing the typical Propagation Delay for the 81110A/11A.

FAQ 2012-02-17

Typical Propagation Delay for the 81110A/12A
Refer to the image showing the Typical Propagation Delay for the 81110A/12A.

FAQ 2012-02-17

M8190A 12 GSa/s Arbitrary Waveform Generator
March 1st question and answer session

FAQ 2011-03-07

PDF PDF 178 KB
Using the 81150A as an arbitrary waveform generator
Although the 81150A is an arbitrary function generator (AFG), it can be used as an arbitrary waveform generator (AWG) with some limits. The key difference between an AFG and an AWG is how data for a digital-to-analog converter is internally genera...

FAQ 2010-07-23

How can I generate de-emphasized signals like they are used e.g. for PCI-Express signalling?
Click above for the answer

FAQ 2010-04-12

81100 Family: Self test fails
The unit is not defective, this behavior is a result of the extensive self tests.

FAQ 2010-04-09

키사이트 N4903A가 라이센스 옵션을 모두 잃었습니다. 복구할 수 있나요?

FAQ 2009-08-10

Channel 2 Output Controls
Please verify how many output modules are installed!

FAQ 2008-11-05

Simplified 8110A, 81101A, 81104A/05A, 81110A/11A Output Schematic
Refer to the Simplified Output Schematic for 8110A, 81101A, 81104A/ 05A,and 81110A/ 11A.

FAQ 2008-11-05

81110A/11A/12A Complement/Differential output
The normal and complementary signals apply only to the 81110A mainframe if the 81112A output module is installed…

FAQ 2008-11-05

8114A의 Variable Baseline 옵션 001은 무엇인가?
표준 8114A에서 베이스라인은 0V로 고정됩니다. 출력 펄스는 선택한 극성에 따라 이 베이스라인의 양의 값이거나 음의 값입니다. -25V부터 +25V까지 베이스라인이 가변적일 수 있도록 하려면8114A에 옵션 001을 장착해야 합니다. 출력 신호는 이 베이스라인을 기준으로 양의 값일 수도 음의 값일 수도 있습니다.

FAQ 2008-05-03

Why isn’t the screen bigger?
The screen is optimized for the “typical” engineering environment where the instrument is up on a lab desk you need to read the numbers from the screen from any angle. In case you need a bigger screen you can manage and control the instrument from...

FAQ 2008-02-21

Why are you offering 3 instruments in 1? What if my customer needs only one of these instruments?
In addition to precise pulses and trigger customers need to stress the device to its limits. In the past they used either a second channel or an additional instrument to distort the signal. With the new build-in capabilities real-world signals can...

FAQ 2008-01-29

What is a crest factor?
The crest factor defines the ratio between Vp to RMS. The ideal sine wave for example has a crest factor of 1.414. Any crest factor higher than 1.414 shows additional noise, distortion or spikes. In addition the crest factor shows signal boundar...

FAQ 2008-01-29

I have a Keysight Pulse Generator, Why shall I buy this new instrument?
In addition to Keysight’s proven Pulse Generator the 81150A provides distortion & modulation capabilities. This gives you complete new test possibilities. In addition the instruments provides coupling & uncoupling of channels. With the coupling you...

FAQ 2008-01-29

How to upgrade from 1 to 2 channels
It is not possible to upgrade a 1 channel version to a 2 channel version. You have to decide from the beginning how many channels you need.

FAQ 2008-01-29

What does channel add mean?
You can add the signal from one channel to the signal of the other channel this might be adding noise to a clean pulse, this might be a FM signal added with noise… The possibilities you have are huge.

FAQ 2008-01-29

Programming the 8114A in terms of current

FAQ 2002-07-03

1 2 다음