Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 78

Sort:
All N603x Arbitrary Waveform Generators IVI and MATLAB Instrument Drivers
Supported models: N6030A, N6031A, N6032A, N6033A

FAQ 2014-08-12

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

What are the Factory Upgrade options for the N6030A?
List of options for M9330A factory upgrades.

FAQ 2014-05-01

What are the Factory Upgrade options for the N8241A and N8242A?
List of options for N8241A and N8242A factory upgrades.

FAQ 2014-05-01

What are the Factory Upgrade options for the M9330A?
List of options for M9330A factory upgrades.

FAQ 2014-05-01

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

Can I turn off the N6030A arbitrary waveform generator predistortion from the N7620B Signal Studio for Pulse Building to get more power?
No. The N7620B software does not allow the N6030A predistortion to be turned off.

FAQ 2012-12-30

Does the Signal Studio for Pulse Building software run on a National Instruments embedded PXI controller like the one that comes with the N6030A?
Yes, it does. However, the Keysight I/O Libraries may need to be installed as a secondary VISA and then the NI Tulip DLL may need to be enabled.

FAQ 2012-12-30

Can multiple software applications communicate with a single N6030A arbitrary waveform generator at the same time?
Only one software application can communicate with the N6030A at a time.

FAQ 2012-12-28

What is the performance difference between the N8212A module with Option 016 and the N8241A arbitrary waveform generator synthetic instrument module?
The N8212A with Option 016 is based on the E8267D PSG signal generator with Option 016; the N8241A is based on the N6030A arbitrary waveform generator.

FAQ 2012-12-28

What is the difference between the 33500A Series and the 33500B Series waveform generators?
Find Information on difference between the 33500A Series and the 33500B Series waveform generators....

FAQ 2012-12-17

Can I upgrade my 33500B Series waveform generator to get additional capability?
Find Information on upgrading the 33500B Series waveform generators for additional capability...

FAQ 2012-12-17

How do I find or confirm my model number, serial number, and configuration of options and upgrades on a 33500B Series waveform generator?
Find information on model number, serial number and configuration of options on the 33500B Series waveform generators...

FAQ 2012-12-11

Is the 33500A and 33500B Series programming code compatible with the 33200 Series programming code?
Find information on the 33500A and 33500B Series programming code compatibility with the 33200 Series programming code...

FAQ 2012-12-11

Can I synchronize functions or arbitrary waveforms on the 33500B Series 2-channel models?
Find Information on synchronizing the 33500B Series 2-channel models....

FAQ 2012-12-11

Can I add two signals together with a magnitude ratio between them? Or what is Sum modulation on the 33500B Series waveform generator?
Find information on adding two signals together on the 33500B Series waveform generators...

FAQ 2012-12-11

How do I create a waveform sequence on the 33500B Series waveform generators?
Find information on how to create a waveform sequence on the 33500B Series waveform generators…

FAQ 2012-12-11

Where is the cfunc.h header file called for in the 33120A Users Guide example program?
Some older versions of the IB Libraries provided this header file during installation. This file was required to access commands from the IB command library.

FAQ 2012-09-05

How Do I Find My Host Information?
The Host ID is the model and/or serial number of the product, both of which can be found on the serial number label on the back of the instrument.

FAQ 2012-06-14

Keysight Driver Migration Tool

FAQ 2012-01-20

N603xA Frequently Asked Questions
N603xA Frequently Asked Questions

FAQ 2011-04-04

N8241A/N8242A Frequently Asked Questions

FAQ 2010-11-22

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

How do I rack mount two instruments of different depths?
There are three ways to rack instruments of different depths side-by-side; for example, a Keysight 33220A with a Keysight 34401A.

FAQ 2010-10-12

What type of internal memory is installed into the 33520A-Series Function/Arbitrary Waveform Generators?
Please refer to the document linked to this page for a comprehensive listing of memory installed into the Keysight 33520A-Series Function / Arbitrary Waveform Generators

FAQ 2010-08-09

1 2 3 4 Next