Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

126-132 de 132

Sort:
VISA COM and IVI-COM Driver: 33220 Square Burst
This program sets up a triggered burst that outputs three cycles of a square wave upon receipt of each trigger.

Exemplo de programação 2003-03-01

VISA COM: 33120 Damped Sine
Demonstrates creating a damped sine wave in an array of integers and then downloading the array as a binary IEEE 488.2 data block.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM: 33250 AsciiArb (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

Programming USB Instruments: Frequency Sweep Sample (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 Haversine
This program sets up a burst waveform with a 270 degree starting phase. By adding an offset voltage to the burst, a haversine is created. This program also shows the use of a trigger received over the GPIB interface to initiate a single trigger.

Exemplo de programação 2003-03-01

VISA COM: 33120 Apply Burst
Demonstrates the use of the Apply command and how to create a burst as an output.

Exemplo de programação 2003-03-01

Test and Measurement World article, Filter Your Data in Software
FIR Filter Software

Exemplo de programação 2002-03-15

Voltar 1 2 3 4 5 6