Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

101-125 de 132

Sort:
VISA COM and IVI-COM Driver: 33250 Linear Sweep (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 Square Burst
This program sets up a triggered burst that outputs three cycles of a square wave upon receipt of each trigger. It will also show how to adjust duty cycle and enable/disable the SYNC output.

Exemplo de programação 2003-03-01

Programming USB Instruments: Frequency Sweep Sample
This program shows how to download an arbitrary waveform using binary data.

Exemplo de programação 2003-03-01

VISA COM: 33120 Apply Burst (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 Linear Sweep
This program sets up a linear sweep using a sinusoid waveform.

Exemplo de programação 2003-03-01

VISA COM: 33120 AM
Demonstrates how to program the instrument for AM modulation and how to store the instrument state in memory.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 Pulse Width
This program uses low-level SCPI commands to configure the function generator to output a PWM waveform.

Exemplo de programação 2003-03-01

VISA COM: 33120 FM (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 AM Waveform and State Storage
This program uses low-level SCPI commands to configure the function generator to output an AM waveform and also shows how to use state storage to store the instrument configuration in memory.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 AsciiArb
This program uses the arbitrary waveform function to download and output a square wave pulse with a calculated rise time and fall time.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 AM Waveform and State Storage (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 Low Level SCPI Commands (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

SICL: *IDN? and Device Info Query on a USB Device (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM: 33120 Damped Sine (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 Haversine (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 Low Level SCPI Commands
This program uses low-level SCPI commands to configure the function generator to output an AM waveform.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 Haversine
This program sets up a burst waveform with a 270 degree starting phase. By adding an offset voltage to the burst, a haversine is created. This program also shows the use of a trigger received over the GPIB interface to initiate a single trigger.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 Pulse Waveshape
This program sets up a pulse waveshape and adjusts the edge time. It also shows the use of high and low voltage levels and period. The edge time is adjusted by 10 nsec increments.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 BinaryArb
This program shows how to download an arbitrary waveform using binary data. The program generates a damped sine wave using 16,000 points.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 Linear Sweep
This program sets up a linear sweep using a sinusoid waveform. It sets the start and stop frequency and sweep time.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33250 Simple Sine (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM Driver: 33220 Linear Sweep (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM: 33120 AM (Read Me)
Code sample documentation.

Exemplo de programação 2003-03-01

VISA COM and IVI-COM: 33250 AsciiArb
This program uses the arbitrary waveform function to download and output a square wave pulse with a calculated rise time and fall time. The waveform consists of 4000 points downloaded to the function generator as ASCII data.

Exemplo de programação 2003-03-01

SICL: *IDN? and Device Info Query on a USB Device
This program opens a communication session with a USB device, does a *IDN? query of the device and gets and displays some device information.

Exemplo de programação 2003-03-01

Voltar 1 2 3 4 5 6 Avançar